[#6624] gcc test on elf-jtag stucks and can't finish

Document created by Aaronwu Employee on Oct 17, 2013
Version 1Show Document
  • View in full screen mode

[#6624] gcc test on elf-jtag stucks and can't finish

Submitted By: Mingquan Pan

Open Date

2011-06-03 03:41:55     Close Date

2011-06-22 10:03:50

Priority:

Medium     Assignee:

Stuart Henderson

Board:

N/A     Silicon Revision:

Resolution:

Duplicate     Fixed In Release:

N/A

Processor:

ALL     

Host Operating System:

toolchain rev.:

head     kernel rev.:

State:

Closed     Found In Release:

2011R1

Is this bug repeatable?:

N/A     

Summary: gcc test on elf-jtag stucks and can't finish

Details:

 

gcc test on elf-jtag stucks and can't finish.

 

Some of the gcc case can pass by testing on elf-jtag, while some still have issues and stops there.

 

Post the logs for bf537-stamp.

 

 

Follow-ups

 

--- Mike Frysinger                                           2011-06-03 09:41:39

i dont think this is a problem with the test script.  i'm not investigating

actual toolchain failures ...

 

--- Stuart Henderson                                         2011-06-22 10:00:56

This is actually a manifestation of [#6135], which turns out to be a testing bug

in dejagnu.  The tests aren't actually sticking, they're just crawling

incredibly slowly as each time we hit the problem we have to wait until it times

out.

 

I'm going to close this as duplicate to keep the discussion in that thread.

 

 

 

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

 

File Name     File Type     File Size     Posted By

gcc.tar.gz    application/gzipped-tar    240552    Mingquan Pan

Attachments

Outcomes