[#6689] gnICE+ fails to be connected to board correctly now

Document created by Aaronwu Employee on Oct 17, 2013
Version 1Show Document
  • View in full screen mode

[#6689] gnICE+ fails to be connected to board correctly now

Submitted By: Mingquan Pan

Open Date

2011-07-14 03:25:48     Close Date

2011-07-18 03:46:50

Priority:

Medium     Assignee:

Jie Zhang

Board:

N/A     Silicon Revision:

Resolution:

Assigned (Not Started)     Fixed In Release:

N/A

Processor:

ALL     

Host Operating System:

toolchain rev.:

    kernel rev.:

State:

Closed     Found In Release:

2011R1

Is this bug repeatable?:

N/A     

Summary: gnICE+ fails to be connected to board correctly now

Details:

 

gnICE+ fails to be connected to board correctly now.

 

Starting start_gdbproxy.exp

 

************** STEP 1: Run start gdbproxy.

 

spawn su^M

Password: ^M

^[[?1034h^[[1m^[[31m46-bf561-gdbproxy:/home/test/work/cruise/test_scripts/toolchain/toolchain-build/toolchain-2011_Jun_01_15_12/bfin-elf/bin # ^[(B^[[msu success.

ps aux| grep bfin-gdbproxy | grep -v grep^M

^[[1m^[[31m46-bf561-gdbproxy:/home/test/work/cruise/test_scripts/toolchain/toolchain-build/toolchain-2011_Jun_01_15_12/bfin-elf/bin # ^[(B^[[m./bfin-gdbproxy bfin^M

^M

Remote proxy for GDB, v0.7.2, Copyright (C) 1999 Quality Quorum Inc.^M

MSP430 adaption Copyright (C) 2002 Chris Liechti and Steve Underwood^M

Blackfin adaption Copyright (C) 2008 Analog Devices, Inc.^M

^M

GDBproxy comes with ABSOLUTELY NO WARRANTY; for details^M

use `--warranty' option. This is Open Source software. You are^M

welcome to redistribute it under certain conditions. Use the^M

'--copying' option for details.^M

^M

Found USB cable: gnICE+^M

Connected to libftdi driver.^M

/home/test/work/cruise/checkouts/toolchain/urjtag/src/tap/discovery.c:117 urj_tap_detect_register_size() Warning: TDO seems to be stuck at 1^M

error:     bfin: detecting parts failed^M

Found USB cable: gnICE+^M

Couldn't connect to suitable USB device.^M

error:     bfin: cable initialization failed^M

Found USB cable: gnICE+^M

Couldn't connect to suitable USB device.^M

error:     bfin: cable initialization failed^M

Found USB cable: gnICE+^M

Couldn't connect to suitable USB device.^M

error:     bfin: cable initialization failed^M

Found USB cable: gnICE+^M

Couldn't connect to suitable USB device.^M

 

Follow-ups

 

--- Mingquan Pan                                             2011-07-18 03:43:16

It turns out to be a power supply issue. Jtag can work now by changing to use

another power bar.

 

spawn su

46-bf561-gdbproxy:/home/test/work/cruise/test_scripts/toolchain/toolchain-build/toolchain-2011_Jun_01_15_12/bfin-elf/bin

# Fail to su.su success.

ps aux| grep bfin-gdbproxy | grep -v grep

46-bf561-gdbproxy:/home/test/work/cruise/test_scripts/toolchain/toolchain-build/toolchain-2011_Jun_01_15_12/bfin-elf/bin

# ./bfin-gdbproxy bfin

 

Remote proxy for GDB, v0.7.2, Copyright (C) 1999 Quality Quorum Inc.

MSP430 adaption Copyright (C) 2002 Chris Liechti and Steve Underwood

Blackfin adaption Copyright (C) 2008 Analog Devices, Inc.

 

GDBproxy comes with ABSOLUTELY NO WARRANTY; for details

use `--warranty' option. This is Open Source software. You are

welcome to redistribute it under certain conditions. Use the

'--copying' option for details.

 

Found USB cable: gnICE+

Connected to libftdi driver.

IR length: 10

Chain length: 2

Device Id: 01010010011110111011000011001011 (0x527BB0CB)

  Manufacturer: Analog Devices, Inc. (0x0CB)

  Part(0):      BF561 (0x27BB)

  Stepping:     5

  Filename:     ./../share/urjtag/analog/bf561/bf561

Device Id: 01010010011110111011000011001011 (0x527BB0CB)

  Manufacturer: Analog Devices, Inc. (0x0CB)

  Part(1):      BF561 (0x27BB)

  Stepping:     5

  Filename:     ./../share/urjtag/analog/bf561/bf561

warning:   bfin: no board selected, 2 cores are detected

warning:   bfin:   cores: [BF561 BF561]

notice:    bfin: jc: waiting on TCP port 2001

notice:    bfin: jc:  (you must connect GDB before using jtag console)

notice:    bfin-gdbproxy: waiting on TCP port 2000

 

 

So close.

 

 

 

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

 

File Name     File Type     File Size     Posted By

No Files Were Found

Attachments

    Outcomes