[#6876] gcc.target case fail tested with rpm package

Document created by Aaronwu Employee on Oct 17, 2013
Version 1Show Document
  • View in full screen mode

[#6876] gcc.target case fail tested with rpm package

Submitted By: Mingquan Pan

Open Date

2011-11-14 00:11:41     Close Date

2011-11-14 08:30:54

Priority:

Medium     Assignee:

Mingquan Pan

Stuart Henderson

Board:

N/A     Silicon Revision:

Resolution:

Rejected     Fixed In Release:

N/A

Processor:

ALL     

Host Operating System:

toolchain rev.:

    kernel rev.:

State:

Closed     Found In Release:

N/A

Is this bug repeatable?:

N/A     

Summary: gcc.target case fail tested with rpm package

Details:

 

gcc.target case fail tested with rpm package. They pass when testing on toolchain built from build script directly.

 

+FAIL: gcc.target/bfin/mcpu-bf504.c (test for excess errors)

+FAIL: gcc.target/bfin/mcpu-bf506.c (test for excess errors)

+FAIL: gcc.target/bfin/mcpu-bf592.c (test for excess errors)

 

spawn bfin-uclinux-gcc /home/test/work/cruise/checkouts/toolchain/gcc-4.3/gcc/testsuite/gcc.target/bfin/mcpu-bf592.c -DSTACK_SIZE=75000 -DNO_TRAMPOLINES -fno-show-column -E -mcpu=bf592 -o mcpu-bf592.i^M

/home/test/work/cruise/checkouts/toolchain/gcc-4.3/gcc/testsuite/gcc.target/bfin/mcpu-bf592.c:14: error: #error "__SILICON_REVISION__ is not 0x0002"^M

compiler exited with status 1

output is:

/home/test/work/cruise/checkouts/toolchain/gcc-4.3/gcc/testsuite/gcc.target/bfin/mcpu-bf592.c:14: error: #error "__SILICON_REVISION__ is not 0x0002"^M

 

FAIL: gcc.target/bfin/mcpu-bf592.c (test for excess errors)

Excess errors:

/home/test/work/cruise/checkouts/toolchain/gcc-4.3/gcc/testsuite/gcc.target/bfin/mcpu-bf592.c:14: error: #error "__SILICON_REVISION__ is not 0x0002"

 

It is tested on :

 

CPU:   ADSP bf548-0.0 (Detected Rev: 0.2) (parallel flash boot)^M

Board: ADI BF548 EZ-Kit board^M

       Support:

Board type is BF548.

http://blackfin.uclinux.org/^M

Clock: VCO: 525 MHz, Core: 525 MHz, System: 131.250 MHz^M

RAM:   64 MiB^M

Flash: 16 MiB^M

NAND:  256 MiB^M

MMC:  Blackfin SDH: 0^M

In:    serial^M

Out:   serial^M

Err:   serial^M

KGDB:  [on serial] ready^M

Net:   smc911x-0^M

Hit any key to stop autoboot:  5 ^H^H^H 0 ^

 

Follow-ups

 

--- Stuart Henderson                                         2011-11-14 08:43:03

these are recently added silicon revisions so won't work with older versions of

the toolchain.  please test with 2011R1-RC3 or trunk.

 

 

 

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

 

File Name     File Type     File Size     Posted By

No Files Were Found

Attachments

    Outcomes