[#7281] bfin-jtag fails to flash u-boot on bf533-stamp

Document created by Aaronwu Employee on Oct 17, 2013
Version 1Show Document
  • View in full screen mode

[#7281] bfin-jtag fails to flash u-boot on bf533-stamp

Submitted By: Mingquan Pan

Open Date

2012-08-23 02:52:07     Close Date

2012-09-17 06:05:55

Priority:

High     Assignee:

Jie Zhang

Board:

N/A     Silicon Revision:

Resolution:

Fixed     Fixed In Release:

N/A

Processor:

ALL     

Host Operating System:

toolchain rev.:

    kernel rev.:

State:

Closed     Found In Release:

2012R2

Is this bug repeatable?:

N/A     

Summary: bfin-jtag fails to flash u-boot on bf533-stamp

Details:

 

bfin-jtag fails to flash u-boot on bf533-stamp.

 

test@adsl:/opt/uClinux/bfin-elf/bin> sudo bfin-jtag

 

UrJTAG 0.10 #

Copyright (C) 2002, 2003 ETC s.r.o.

Copyright (C) 2007, 2008, 2009 Kolja Waschk and the respective authors

 

UrJTAG is free software, covered by the GNU General Public License, and you are

welcome to change it and/or distribute copies of it under certain conditions.

There is absolutely no warranty for UrJTAG.

 

warning: UrJTAG may damage your hardware!

Type "quit" to exit, "help" for help.

 

jtag> cable probe

Found USB cable: gnICE

Connected to libftdi driver.

jtag> detect

IR length: 5

Chain length: 1

Device Id: 00110010011110100101000011001011 (0x327A50CB)

  Manufacturer: Analog Devices, Inc. (0x0CB)

  Part(0):      BF533 (0x27A5)

  Stepping:     3

  Filename:     ../share/urjtag/analog/bf533/bf533

jtag> initbus bf533_stamp

jtag> detectflash 0x20000000

dev ID=0fec   man ID=e10e

urj_flash_amd_detect: mid e10e, did e10e

error: flash: mid != 0x01

 

test@adsl:/opt/uClinux/bfin-elf/bin> /opt/uClinux/bfin-elf/bin/bfin-elf-gcc -v

Using built-in specs.

Target: bfin-elf

Configured with: /usr/src/packages/BUILD/blackfin-toolchain-2012R1/gcc-4.3/configure --build=i686-pc-linux-gnu --host=i686-pc-linux-gnu --target=bfin-elf --prefix=/opt/uClinux/bfin-elf --disable-libstdcxx-pch --enable-languages=c,c++ --with-newlib --enable-clocale=generic --disable-symvers --disable-libssp --disable-libffi --disable-libgcj --enable-version-specific-runtime-libs --enable-__cxa_atexit --with-bugurl=URL:http://blackfin.uclinux.org/gf/project/toolchain/tracker --with-pkgversion=ADI-2012R1-ALPHA2

Thread model: single

gcc version 4.3.5 (ADI-2012R1-ALPHA2)

 

Follow-ups

 

--- Jie Zhang                                                2012-09-12 16:40:39

should be fixed now. please verify.

 

--- Mingquan Pan                                             2012-09-17 07:06:50

Yes, it can flash uboot on bf533 stamp now. close.

 

 

 

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

 

File Name     File Type     File Size     Posted By

No Files Were Found

Attachments

    Outcomes