[#7292] Blackfin GNU tool chain Eclipse plug-in reports "WARNING: The "Debug" Configuration may not build"

Document created by Aaronwu Employee on Oct 17, 2013
Version 1Show Document
  • View in full screen mode

[#7292] Blackfin GNU tool chain Eclipse plug-in reports "WARNING: The "Debug" Configuration may not build"

Submitted By: Andrew McLachlan

Open Date

2012-08-27 06:59:30     Close Date

2012-08-30 08:55:14

Priority:

Medium     Assignee:

Andrew McLachlan

Board:

N/A     Silicon Revision:

Resolution:

Fixed     Fixed In Release:

N/A

Processor:

ALL     

Host Operating System:

All

toolchain rev.:

    kernel rev.:

State:

Closed     Found In Release:

2012R1

Is this bug repeatable?:

N/A     

Summary: Blackfin GNU tool chain Eclipse plug-in reports "WARNING: The "Debug" Configuration may not build"

Details:

 

1, Install the Blackfin GNU tool chain Eclipse plug-ins into Juno

2, Create a new "Blackfin Linux FDPIC GNU Toolchain (bfin-linux-uclibc)" project for BF538

3, Build the project

 

**** Build of configuration Debug for project test ****

 

****  WARNING: The "Debug" Configuration may not build  ****

****  because it uses the "Blackfin Linux FDPIC GNU Toolchain (bfin-linux-uclibc)"  ****

****  tool-chain that is unsupported on this system.  ****

 

****  Attempting to build...  ****

 

make all

'Building file: ../system/adi_initialize.c'

'Invoking: Blackfin FDPIC C Compiler'

bfin-linux-uclibc-gcc -D_DEBUG -I"C:\Users\amclach\Desktop\CCES Workspace\test\system" -O0 -g3 -Wall -c -fmessage-length=0 -mcpu=bf549m-any -MMD -MP -MF"system/adi_initialize.d" -MT"system/adi_initialize.d" -o "system/adi_initialize.o" "../system/adi_initialize.c"

'Finished building: ../system/adi_initialize.c'

' '

'Building file: ../src/test.c'

'Invoking: Blackfin FDPIC C Compiler'

bfin-linux-uclibc-gcc -D_DEBUG -I"C:\Users\amclach\Desktop\CCES Workspace\test\system" -O0 -g3 -Wall -c -fmessage-length=0 -mcpu=bf549m-any -MMD -MP -MF"src/test.d" -MT"src/test.d" -o "src/test.o" "../src/test.c"

'Finished building: ../src/test.c'

' '

'Building target: test'

'Invoking: Blackfin FDPIC C Linker'

bfin-linux-uclibc-gcc -mcpu=bf549m-any -o "test"  ./system/adi_initialize.o  ./src/test.o  

'Finished building target: test'

' '

 

The issue is that the `bfin-linux-uclibc-ldr` command has not been filled in for the Blackfin Loader Tools Settings.

 

Workaround: add bfin-linux-uclibc-ldr explicitly to command entry box.

 

Additional: the Loader settings are not necessarily needed for this type of project set-up.

Ideally, we'd have an "Artifact type: Loader file" and make visible|enable/invisible|disable

the Loader tools settings according to the Artifact selection.

 

 

Follow-ups

 

--- Andrew McLachlan                                         2012-08-30 09:53:26

 

  Fixed in Blackfin GNU tool chain Eclipse plug-in v1.0.6.

 

 

 

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

 

File Name     File Type     File Size     Posted By

No Files Were Found

Attachments

    Outcomes