[#7318] Ensure that -mmulticore -mcore0 is set on Eclipse ADSP-BF561/BF60x project creation

Document created by Aaronwu Employee on Oct 17, 2013
Version 1Show Document
  • View in full screen mode

[#7318] Ensure that -mmulticore -mcore0 is set on Eclipse ADSP-BF561/BF60x project creation

Submitted By: Andrew McLachlan

Open Date

2012-09-11 05:32:22     Close Date

2012-10-10 03:32:56

Priority:

Medium High     Assignee:

Andrew McLachlan

Board:

N/A     Silicon Revision:

Resolution:

Fixed     Fixed In Release:

N/A

Processor:

ALL     

Host Operating System:

toolchain rev.:

    kernel rev.:

State:

Closed     Found In Release:

2012R1

Is this bug repeatable?:

N/A     

Summary: Ensure that -mmulticore -mcore0 is set on Eclipse ADSP-BF561/BF60x project creation

Details:

 

#7317 and #7313 outline an issue with running a program on Core 0 that could

have easily been avoided.

 

Although #7317 (GCC should generate code for Core 0 by default) would mean that

an out-of-the box BF609 single project would run on Core 0, an App-per-core

project set-up would fail, if we were to create two projects.

 

We therefore require the setting of "-mmulticore -mcore0" during New project

creation in Eclipse too. And, perhaps, the ability to toggle the core nicely

in the Tools Settings.

 

 

 

Follow-ups

 

--- Andrew McLachlan                                         2012-10-10 04:34:27

 

Fixed in plug-ins version 1.0.7.

 

 

 

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

 

File Name     File Type     File Size     Posted By

No Files Were Found

Attachments

    Outcomes