FAQ: ADIS16405 Magnetometer Bias Errors

Document created by NevadaMark Employee on Oct 14, 2013
Version 1Show Document
  • View in full screen mode

Q:

What can cause very large offset errors in the ADIS16405 magnetometer outputs?

---------------------------------------------------------------------------------------------------------------------

A:

One potential cause is through magnetizing internal materials.  This happens when devices experience high-intensity magnetic fields, typically in excess of 20 Gauss. Fortunately, these units can be "de-magnetized" using relatively simple equipment. The following videos illustrate both hand-held and bench-top processes.  Here are links to more information on the equipment in these videos:

 

Hand-held demagnetizer: http://www.rbannis.com/products/handmags.html

Bench-top demagnetizer: http://www.em-chicago.com/Standard_Surface_Demagnetizers.html

 

The key part of de-magnetizing the ADIS16405 is to expose the device to alternating and decaying magnetic fields.

 

Hand-held Process

The following video shows the hand-motion that we use to de-magnetize an ADIS16405. The combination of circular and raising motion helps create both alternating and decaying fields.

NOTE: Keep the unit away from the probe or turn the probe off if it must return to a location near the unit after completing this process.

 

Bench-top Process

This process is a little simpler. Rotate the device on its surface a few times, then lift it away from the surface of the instrument.

NOTE: Keep the unit away from the demagnetizer surface or turn the instrument off if before returning the unit to a location near the surface.

Attachments

    Outcomes