2010-09-22 08:40:33     Is it possible to automate DDD commands thro scripting?

Document created by Aaronwu Employee on Sep 26, 2013
Version 1Show Document
  • View in full screen mode

2010-09-22 08:40:33     Is it possible to automate DDD commands thro scripting?

Kishore Prahlad (INDIA)

Message: 93743   

 

I am using DDD for debugging the codes.....

 

the following commands are given in DDD to run the code in the target board

 

target remote <ip address of the board>:port number used(before giving this i would star the GDB server with the same port number to listen)

 

everytime I need to give this to start debugging the code.Is there anyway by which I can put these commands into a script and automate the process........

 

Actually we are trying to develop a system where we have a set of boards and thro the network we are trying to access them.When some board is free we wanted to allocate it for a user who is waiting in the queue,To make the interface simpler we dont want the user to give  all these commands from their end.

 

Need some suggestions on whether automating these commands are possible or not

 

thanks

QuoteReplyEditDelete

 

 

2010-09-22 13:36:02     Re: Is it possible to automate DDD commands thro scripting?

Mike Frysinger (UNITED STATES)

Message: 93763   

 

ddd is simply a gui frontend to gdb.  all of the gdb scripting works the same under ddd.

Attachments

    Outcomes