2010-09-08 03:03:58     malloc.h clarification

Document created by Aaronwu Employee on Sep 26, 2013
Version 1Show Document
  • View in full screen mode

2010-09-08 03:03:58     malloc.h clarification

svs k (INDIA)

Message: 93237   


Hi All,




Kindly tell me if the following functions are supported in 2009R1.1-RC2 or any other toolchains. I could not see the declarations in malloc.h file. I currently have a file that has the following functions and not able to compile the file in blackfin  gcc toolchain. but the file is compiling in gcc toolchain.  Kindly clarify how can i compile the file with the existing bfin gcc toolchain.




void * (*malloc_hook)(size_t s);

  void * (*realloc_hook)(void *p , size_t s );

  void (*free_hook)(void *p );

  void * (*memalign_hook)(size_t al, size_t s );











2010-09-08 03:09:41     Re: malloc.h clarification

Mike Frysinger (UNITED STATES)

Message: 93238   


there is no support for those non-standard hooks nor will there ever be