FAQ:  Why are certain portions of my EZ-KIT Lite schematics missing or not shown?

Document created by mue on Apr 13, 2009Last modified by CraigG on Aug 24, 2012
Version 4Show Document
  • View in full screen mode

Q:

The BF548 EZ-KIT Lite schematic is missing the Debug Agent interface. Is this part of the schematic available?

 

----------

 

A:

The Debug Agent (USB debugger) interface on the EZ-KIT Lite is proprietary. This is implemented by the FPGA and, on newer EZ-KIT Lites, additional BF535 processor.


What is not shown on the schematics:
The EZ-Kit includes hardware consisting of an FPGA on older EZ-KIT Lites, and a BF535 on newer EZ-KIT Lites,  which implements two different main  functions. It implements a proprietary USB debugger interface for communication between the board and the host PC as well as also implementing a serial port interface for communication between the DSPs and the on-board converters.

 

 

Further details of the FPGA/BF535 interface (software and hardware) of this undisclosed section of the EZ-Kit Lite are proprietary and cannot be made available.

 

Additionally, board design information for all released products can be found via the "EZ-KIT Lite Design Database" link on the Product Information page for the appropriate EZ-KIT Lite, as well as being available at the following locations:

21xx Board Design Database

TigerSHARC Board Design Database

SHARC Board Design Database

Blackfin Board Design Database

 

Please refer to the Readme.txt for a description of the contents of the ZIP files.

 

----------

 

This FAQ was generated from the following thread: Why are certain portions of my EZ-KIT Lite schematics missing or not shown?

Attachments

    Outcomes