2010-06-02 11:46:16     Kernel build fails to complete, but doesn't give any proper error message

Document created by Aaronwu Employee on Sep 26, 2013
Version 1Show Document
  • View in full screen mode

2010-06-02 11:46:16     Kernel build fails to complete, but doesn't give any proper error message

Abhinay Patil (INDIA)

Message: 90075   

 

Hi,

 

       I am trying to build the uClinux kernel but the build terminates abruptly without giving any meaningful error message. I am at a loss to understand where I am going wrong. Here's the procedure I followed:

 

1. Downloaded and untarred latest uClinux distribution

 

2. Downloaded and installed latest toolchain and uclibc

 

3. Set PATH variable

 

4. Performed "Make menuconfig". Selected vendor as Analog Devices and Product as BF-537 Stamp. I selected Linphone from the list of canned applications. All the other settings were left at default.

 

5. Performed make

 

    After this, I see the kernel build in progress which progresses a long way before terminating abruptly. There are no meaningful error messages except "Error 1" and "Error 2". There's nothing preceding these error messages which indicate the reason for the failure.

 

   Can you please help me to build the kernel successfully?

 

Thanks and regards,

 

Abhinay

 

Analog Devices India

QuoteReplyEditDelete

 

 

2010-06-02 15:24:43     Re: Kernel build fails to complete, but doesn't give any proper error message

Mike Frysinger (UNITED STATES)

Message: 90076   

 

either search the whole log for the error message or run `make single`

Attachments

    Outcomes