2010-05-12 22:45:12     question about the flat and fdpic elf format

Document created by Aaronwu Employee on Sep 26, 2013
Version 1Show Document
  • View in full screen mode

2010-05-12 22:45:12     question about the flat and fdpic elf format

steven O (AFGHANISTAN)

Message: 89345   

 

fucos on this topic as following :

 

http://blackfin.uclinux.org/gf/project/toolchain/forum/?_forum_action=ForumMessageBrowse&thread_id=23307&action=ForumBrowse

 

has it been solved?  what is the difference between the flat and fdpic elf format?

QuoteReplyEditDelete

 

 

2010-05-13 10:25:06     Re: question about the flat and fdpic elf format

Robin Getz (UNITED STATES)

Message: 89375   

 

Steven:

 

There is nothing to be solved.

 

https://docs.blackfin.uclinux.org/doku.php?id=toolchain:executable_file_formats

QuoteReplyEditDelete

 

 

2010-05-13 22:04:22     Re: question about the flat and fdpic elf format

steven O (AFGHANISTAN)

Message: 89393   

 

There is nothing to be solved ???

 

I had get the same problem now. Can you tell me how to solved it ?  the process of my program was killed, when i used the ftp service to list the files in the harddisk. And what is the meaning of  "crash" in the link? I puzzled in this problem long time. thanks.

QuoteReplyEditDelete

 

 

2010-05-14 11:57:12     Re: question about the flat and fdpic elf format

Robin Getz (UNITED STATES)

Message: 89414   

 

Steven:

 

you are running out of memory - the only solution is to add more.

 

-Robin

QuoteReplyEditDelete

 

 

2010-05-17 04:52:08     Re: question about the flat and fdpic elf format

steven O (AFGHANISTAN)

Message: 89481   

 

i just use the ftpd to list a few files, the shell also do it as the link. and my system has enough free memory (about 41M). i think the ftpd can't use 41M memory at once. So i can't understand the system is running out of memory.

 

Sorry , the kernel of uclinux  is strangeness to me. Please give me more infornation, thanks

QuoteReplyEditDelete

 

 

2010-05-17 05:29:21     Re: question about the flat and fdpic elfformat

Michael Hennerich (GERMANY)

Message: 89483    Instead of referring to an 3 years old unrelated thread - can you provide

more useful information on what you're doing and how it fails.

Please do this in the [uclinux-help] forum.

 

I would also consider this being a stack size issue.

 

http://docs.blackfin.uclinux.org/doku.php?id=uclinux-dist:debugging_applications&s[]=stack

Attachments

    Outcomes