2010-04-02 05:55:57     IPv6 support

Document created by Aaronwu Employee on Sep 26, 2013
Version 1Show Document
  • View in full screen mode

2010-04-02 05:55:57     IPv6 support

Parimala Baggiri (INDIA)

Message: 88027   

 

Hello,

 

How to build the toolchain for the firsttime by enabling IPv6? Is this the config file toolchain/uClibc/extra/Configs/Config.bfin.default to make UCLIBC_HAS_IPV6=y ?

 

Regards,

 

Parimala

QuoteReplyEditDelete

 

 

2010-04-02 06:00:30     Re: IPv6 support

Mike Frysinger (UNITED STATES)

Message: 88029   

 

do not edit the source files directly.  copy the .config file somewhere with your changes and use the -C option to BuildToolChain.

 

see the documentation:

http://docs.blackfin.uclinux.org/doku.php?id=toolchain:buildscript

QuoteReplyEditDelete

 

 

2010-04-02 06:01:58     Re: IPv6 support

Parimala Baggiri (INDIA)

Message: 88030   

 

Forgot to give processor details in the previous message

 

ADSP-BF537STAMP0.3

 

toolchain: svn 3831

QuoteReplyEditDelete

 

 

2010-04-02 06:10:51     Re: IPv6 support

Parimala Baggiri (INDIA)

Message: 88031   

 

Hello Mike,

 

Yes, I have followed the document

 

Building a Toolchain with Locale Support in that link. To build toolchain for the firsttime there will not any .config file.

 

So, twice I have to build toolchain once normally & second time build with the genarated .config with IPv6 enabled.

 

Is it the procedure?

 

Regards,

 

Parimala

QuoteReplyEditDelete

 

 

2010-04-02 06:23:25     Re: IPv6 support

Mike Frysinger (UNITED STATES)

Message: 88033   

 

make the .config file yourself

QuoteReplyEditDelete

 

 

2010-04-02 06:29:13     Re: IPv6 support

Parimala Baggiri (INDIA)

Message: 88034   

 

Hello Mike,

 

Thank you. Which configuration file I need to take as a reference?

QuoteReplyEditDelete

 

 

2010-04-02 12:50:03     Re: IPv6 support

Mike Frysinger (UNITED STATES)

Message: 88044   

 

use the config file you already referenced as a base and create a ful one using make menuconfig

QuoteReplyEditDelete

 

 

2010-04-05 07:10:19     Re: IPv6 support

Parimala Baggiri (INDIA)

Message: 88094   

 

Hello Mike,

 

"use the config file you already referenced as a base" means I need to compile the toolchain twice as mentioned previously or use toolchain/uClibc/extra/Configs/Config.bfin.default as the base config file?

 

I would like to know which is the basic config file BuildScript uses to build toolchain?

QuoteReplyEditDelete

 

 

2010-04-11 16:20:58     Re: IPv6 support

Mike Frysinger (UNITED STATES)

Message: 88300   

 

it's trivial to go into the uClibc directory and run `make config` yourself using the base config file you've already referenced.  if that's too much, then build the toolchain twice.

Attachments

    Outcomes