2010-01-20 02:25:52     U-boot does not build at the end of the tool chain build

Document created by Aaronwu Employee on Sep 26, 2013
Version 1Show Document
  • View in full screen mode

2010-01-20 02:25:52     U-boot does not build at the end of the tool chain build

Mark Noonchester (NEW ZEALAND)

Message: 84787   

 

U-boot does not build at the end of the tool chain build process.

 

However it will build manualy.

 

This ploblem is on os-x 10.6 but it could be on other platforms.

QuoteReplyEditDelete

 

 

2010-01-20 05:09:20     Re: U-boot does not build at the end of the tool chain build

Mark Noonchester (NEW ZEALAND)

Message: 84845   

 

Please report an error to http://blackfin.uclinux.org/gf/project/toolchain

Build error Wed 20 Jan 2010 22:47:23 NZDT

  occurred 1h59m28s into script

tar: Removing leading `/' from member names

When reporting issue, we may ask for /Volumes/beluga-b/blackfin_sources/build_test/logs/config.logs.tbz2

Last logfile entries:

 

sed: can't read include/configs/.h: No such file or directory

Generating /Volumes/beluga-b/blackfin_sources/build_test/u-boot_build/include/autoconf.mk

cc1: error: unrecognized command line option "-mcpu="

for dir in tools cpu/ /Volumes/beluga-b/blackfin_sources/u-boot/u-boot-2009.11/board// ; do \

            make -C $dir _depend ; done

make[1]: Nothing to be done for `_depend'.

make[1]: *** No rule to make target `_depend'.  Stop.

make[1]: *** No rule to make target `_depend'.  Stop.

make: *** [depend] Error 2

 

log.20100120.zip

QuoteReplyEditDelete

 

 

2010-01-20 07:53:51     Re: U-boot does not build at the end of the tool chain build

Mike Frysinger (UNITED STATES)

Message: 84851   

 

probably want to revert the recent commit:

Makefile: fix parallel build

svn rev 2211

QuoteReplyEditDelete

 

 

2010-01-20 16:25:35     Re: U-boot does not build at the end of the tool chain build

Mark Noonchester (NEW ZEALAND)

Message: 84867   

 

I am using the latest version of u-boot and this does not help are you saing to use version 2211 of u-boot?

QuoteReplyEditDelete

 

 

2010-01-20 16:29:05     Re: U-boot does not build at the end of the tool chain build

Jie Zhang (UNITED STATES)

Message: 84868   

 

No. You need to revert what 2211 changed. Or you can simply checkout 2210.

QuoteReplyEditDelete

 

 

2010-01-20 22:55:44     Re: U-boot does not build at the end of the tool chain build

Mark Noonchester (NEW ZEALAND)

Message: 84873   

 

Thanks that works great.

QuoteReplyEditDelete

 

 

2010-01-21 03:26:21     Re: U-boot does not build at the end of the tool chain build

Mike Frysinger (UNITED STATES)

Message: 84926   

 

latest u-boot/toolchain svn trunk should work again

QuoteReplyEditDelete

 

 

2010-01-21 14:49:54     Re: U-boot does not build at the end of the tool chain build

Mark Noonchester (NEW ZEALAND)

Message: 84945   

 

Thanks Mike the curent system now builds

Attachments

Outcomes