[#7798] u-boot run on bf609-ezkit with 0.1 chip still detected as 0.0 chip

Document created by Aaronwu Employee on Sep 26, 2013
Version 1Show Document
  • View in full screen mode

[#7798] u-boot run on bf609-ezkit with 0.1 chip still detected as 0.0 chip

Submitted By: Mingquan Pan

Open Date

2013-05-30 23:46:29    

Priority:

Medium     Assignee:

Sonic Zhang

Category:

N/A     Fixed In Release:

2013R1

Found In Release:

2013R1     Status:

Open

Board:

N/A     Processor:

BF609

Silicon Revision:

0.1     Resolution:

Rejected

Is the bug repeatable?:

N/A     

Summary: u-boot run on bf609-ezkit with 0.1 chip still detected as 0.0 chip

Details:

 

u-boot run on bf609-ezkit with 0.1 chip still detected as 0.0 chip.

 

 

 

BusyBox v1.21.0 (2013-04-14 14:48:31 CST) hush - the humble shell

 

root:/> libphy: stmmac-0:01 - Link is Up - 100/Full

P�턔�

 

U-Boot 2013.04 (ADI-2013R1-pre)-00353-g5a20eb3-dirty (May 31 2013 - 12:52:25)

 

CPU:   ADSP bf609-0.0 (Detected Rev: 0.0) (parallel flash boot)

Board: ADI BF609 EZ-Kit board

       Support: http://blackfin.uclinux.org/

Clock: VCO: 500 MHz, Core: 500 MHz, System0: 125 MHz, System1: 125 MHz, Dclk: 250 MHz

RAM:   128 MiB

Flash: 16 MiB

MMC:   Blackfin SDH: 0

In:    serial

Out:   serial

Err:   serial

KGDB:  [on serial] ready

other init

Net:   mii0

Hit any key to stop autoboot:  0

bfin> sf probe 1

SF: Detected W25Q32 with page size 4 KiB, total 4 MiB

bfin>

 

Follow-ups

 

--- Sonic Zhang                                              2013-06-07 05:29:17

Not a software bug. The CPUID MMR on bf609 rev. 0.1 is read 0.

 

 

 

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

 

File Name     File Type     File Size     Posted By

No Files Were Found

Attachments

    Outcomes