[#7764] fsload uimage easily get hanged on bf609-ezkit

Document created by Aaronwu Employee on Sep 26, 2013
Version 1Show Document
  • View in full screen mode

[#7764] fsload uimage easily get hanged on bf609-ezkit

Submitted By: Mingquan Pan

Open Date

2013-05-06 03:55:47     Close Date

2013-05-16 03:06:12

Priority:

Medium     Assignee:

Sonic Zhang

Category:

N/A     Fixed In Release:

2013R1

Found In Release:

2013R1     Status:

Closed

Board:

N/A     Processor:

BF609

Silicon Revision:

    Resolution:

Not reproducible

Is the bug repeatable?:

N/A     

Summary: fsload uimage easily get hanged on bf609-ezkit

Details:

 

fsload uimage easily get hanged on bf609-ezkit, then make board reset.

 

CPU:   ADSP bf609-0.0 (Detected Rev: 0.0) (parallel flash boot)^M

Board: ADI BF609 EZ-Kit board^M

       Support: http://blackfin.uclinux.org/^M

Clock: VCO: 500 MHz, Core: 500 MHz, System0: 83.333 MHz, System1: 83.333 MHz, Dclk: 250 MHz^M

RAM:   128 MiB^M

Flash: 16 MiB^M

MMC:   Blackfin SDH: 0^M

In:    serial^M

Out:   serial^M

Err:   serial^M

other init^M

Net:   mii0^M

Hit any key to stop autoboot:  9 ^H^H^H 8 ^H^H^H 7 ^H^H^H 6 ^H^H^H 5 ^H^H^H 0 ^M

bfin> waiting for uboot prompt

^M

bfin> got u-boot prompt

icache off^M

bfin> dcache on^M

bfin> reginfo^M

^M

System Configuration registers^M

^M

CGU Registers^M

        CGU_DIV:   0x44022621   CGU_CTL:      0x00001400^M

        CGU_STAT:  0x000003f5   CGU_LOCKCNT:  0x00000000^M

^M

SMC DDR Registers^M

        DDR_CFG:   0x00000422   DDR_TR0:      0x20e0a424^M

        DDR_TR1:   0x3020079e   DDR_TR2:      0x0032050d^M

        DDR_MR:    0x00000842   DDR_EMR1:     0x00000004^M

        DDR_CTL:   0x00000900   DDR_STAT:     0x00402007^M

        DDR_DLLCTL:0x0000044b^M

bfin> ls^M

Scanning JFFS2 FS:   ^H^H.  ^H^H.  ^H^H done.^M^M

drwxr-xr-x        0 Thu May 12 01:54:58 2005 bin^M^M

drwxr-xr-x        0 Thu May 12 01:54:55 2005 dev^M^M

drwxr-xr-x        0 Thu May 12 01:54:58 2005 etc^M^M

drwxr-xr-x        0 Thu May 12 01:54:55 2005 home^M^M

drwxr-xr-x        0 Thu May 12 01:54:55 2005 lib^M^M

drwxr-xr-x        0 Thu May 12 01:54:55 2005 mnt^M^M

drwxr-xr-x        0 Thu May 12 01:54:55 2005 proc^M^M

drwxr-xr-x        0 Thu May 12 01:54:55 2005 root^M^M

lrwxrwxrwx        3 Thu May 12 01:54:55 2005 sbin -> bin^M^M

drwxr-xr-x        0 Thu May 12 01:54:55 2005 tmp^M^M

-rw-r--r--  2261906 Thu May 12 02:34:01 2005 uImage^M^M

drwxr-xr-x        0 Thu May 12 01:54:55 2005 usr^M^M

drwxr-xr-x        0 Thu May 12 01:54:55 2005 var^M^M

bfin> fsinfo^M

### filesystem type is JFFS2^M

Compression: NONE^M

        frag count: 707^M

        compressed sum: 2108941^M

        uncompressed sum: 2108941^M

Compression: ZERO^M

        frag count: 0^M

        compressed sum: 0^M

        uncompressed sum: 0^M

Compression: RTIME^M

        frag count: 0^M

        compressed sum: 0^M

        uncompressed sum: 0^M

Compression: RUBINMIPS^M

        frag count: 0^M

        compressed sum: 0^M

        uncompressed sum: 0^M

Compression: COPY^M

        frag count: 0^M

        compressed sum: 0^M

        uncompressed sum: 0^M

Compression: DYNRUBIN^M

        frag count: 0^M

        compressed sum: 0^M

        uncompressed sum: 0^M

Compression: ZLIB^M

        frag count: 429^M

        compressed sum: 1063884^M

        uncompressed sum: 1615243^M

bfin> fsload /uImage^M

### JFFS2 loading '/uImage' to 0x1000000^M

^M

^M

U-Boot 2013.04 (ADI-2013R1-pre)-00352-g8cec8b3-dirty (May 04 2013 - 13:10:11), Build: jenkins-label=UBOOT_BF609-EZKIT-304^M

^M

CPU:   ADSP bf609-0.0 (Detected Rev: 0.0) (parallel flash boot)^M

Board: ADI BF609 EZ-Kit board^M

       Support: http://blackfin.uclinux.org/^M

Clock: VCO: 500 MHz, Core: 500 MHz, System0: 83.333 MHz, System1: 83.333 MHz, Dclk: 250 MHz^M

RAM:   128 MiB^M

Flash: 16 MiB^M

MMC:   Blackfin SDH: 0^M

In:    serial^M

Out:   serial^M

Err:   serial^M

other init^M

Net:   mii0^M

Hit any key to stop autoboot:  9 ^H^H^H 8 ^H^H^H 7 ^H^H^H 6 ^H^H^H 5 ^H^H^H 4 ^H^H^H 3 ^H^H^H 2 ^H^H^H 1 ^H^H^H 0 ^M

## Booting kernel from Legacy Image at 01000000 ...^M

   Image Name:   Bfin uClinux Kernel^M

   Image Type:   Blackfin Linux Kernel Image (gzip compressed)^M

   Data Size:    2261842 Bytes = 2.2 MiB^M

   Load Address: 00001000^M

   Entry Point:  00001000^M

   Verifying Checksum ... Bad Data CRC^M

ERROR: can't get kernel image!^M

bfin> JFFS2 'ls'     result: pass

JFFS2 'fsinfo' result: pass

JFFS2 'fsload' result: fail

 

===== Recording result: jffs2 is fail

 

 

Follow-ups

 

--- Sonic Zhang                                              2013-05-13 06:02:47

Can't replicate.

May need to enlarge the watchdog timeout value in test script.

 

--- Mingquan Pan                                             2013-05-16 04:13:29

This is due to fsload cost more time which trigger watchdog reset the board.

Enlarge the watchdog timeout fix this.

 

 

 

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

 

File Name     File Type     File Size     Posted By

No Files Were Found

Attachments

    Outcomes