[#7759] cmp result fails on trunk head

Document created by Aaronwu Employee on Sep 26, 2013
Version 1Show Document
  • View in full screen mode

[#7759] cmp result fails on trunk head

Submitted By: Mingquan Pan

Open Date

2013-05-01 21:56:10     Close Date

2013-05-03 01:52:59

Priority:

Medium     Assignee:

Sonic Zhang

Category:

N/A     Fixed In Release:

2013R1

Found In Release:

2013R1     Status:

Closed

Board:

N/A     Processor:

BF609

Silicon Revision:

    Resolution:

Fixed

Is the bug repeatable?:

N/A     

Summary: cmp result fails on trunk head

Details:

 

cmp result fails on trunk head.

 

*****************************

STEP 23: cmp

 

tftp 0x1000000 testfile.bin^M

Waiting for PHY auto negotiation to complete. done^M

ENET Speed is 100 Mbps - FULL duplex connection^M

Using mii0 device^M

TFTP from server 10.100.4.174; our IP address is 10.100.4.50^M

Filename 'testfile.bin'.^M

Load address: 0x1000000^M

Loading: *^H#^M

         2.2 MiB/s^M

done^M

Bytes transferred = 9137 (23b1 hex)^M

bfin>

random SDRAM loc is   0x01020000

random SDRAM len is   0x10000

random SDRAM end is   0x01030000

one before the end is 0x0102ffff

waiting for uboot prompt

cp.b 0x1000000 01020000 10000^M

bfin> got u-boot prompt

icache on^M

bfin> dcache off^M

bfin> reginfo^M

^M

System Configuration registers^M

^M

CGU Registers^M

        CGU_DIV:   0x44022621   CGU_CTL:      0x00001400^M

        CGU_STAT:  0x000003f5   CGU_LOCKCNT:  0x00000000^M

^M

SMC DDR Registers^M

        DDR_CFG:   0x00000422   DDR_TR0:      0x20e0a424^M

        DDR_TR1:   0x3020079e   DDR_TR2:      0x0032050d^M

        DDR_MR:    0x00000842   DDR_EMR1:     0x00000004^M

        DDR_CTL:   0x00000900   DDR_STAT:     0x00402007^M

        DDR_DLLCTL:0x0000044b^M

bfin> cmp.b 0x1000000 01020000 10000^M

byte at 0x01000000 (0x7f) != byte at 0x01020000 (0x32)^M

Total of 0 byte(s) were the same^M

bfin>

===== Recording result: cmp is fail

 

 

Follow-ups

 

--- Mingquan Pan                                             2013-05-03 03:00:11

it is passed on bf537 now.Close.

 

 

 

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

 

File Name     File Type     File Size     Posted By

No Files Were Found

Attachments

    Outcomes