[#7733] fatls show two lines of the same file

Document created by Aaronwu Employee on Sep 26, 2013
Version 1Show Document
  • View in full screen mode

[#7733] fatls show two lines of the same file

Submitted By: Mingquan Pan

Open Date

2013-03-29 03:14:30    

Priority:

Very Low     Assignee:

Nobody

Category:

N/A     Fixed In Release:

2013R1

Found In Release:

2013R1     Status:

Open

Board:

N/A     Processor:

BF527

Silicon Revision:

    Resolution:

N/A

Is the bug repeatable?:

N/A     

Summary: fatls show two lines of the same file

Details:

 

fatls always show two lines of the same file.

 

U-Boot 2013.01 (ADI-2013R1-pre)-00338-gf20bfed-dirty (Mar 27 2013 - 22:59:16),

Build: jenkins-label=UBOOT_BF527-EZKIT-9

 

CPU:   ADSP bf527-0.0 (Detected Rev: 0.2) (parallel flash boot)

Board: ADI BF527 EZ-Kit board

       Support: http://blackfin.uclinux.org/

Clock: VCO: 600 MHz, Core: 600 MHz, System: 50 MHz

RAM:   64 MiB

Flash: 4 MiB

In:    serial

Out:   serial

Err:   serial

KGDB:  [on serial] ready

Net:   bfin_mac

Hit any key to stop autoboot:  0

bfin> usb start

(Re)start USB...

USB0:   scanning bus 0 for devices... 1 USB Device(s) found

       scanning usb for storage devices... 1 Storage Device(s) found

bfin> fatls usb 0   

  5293341   uimage

  5293341   uimage

 

2 file(s), 0 dir(s)

 

 

 

 

Follow-ups

No Messages Were Found

 

 

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

 

File Name     File Type     File Size     Posted By

No Files Were Found

Attachments

    Outcomes