[#7693] spi flash on bf609 ezkit fails to be probed

Document created by Aaronwu Employee on Sep 26, 2013
Version 1Show Document
  • View in full screen mode

[#7693] spi flash on bf609 ezkit fails to be probed

Submitted By: Mingquan Pan

Open Date

2013-03-07 03:06:26     Close Date

2013-04-10 22:32:34

Priority:

Medium     Assignee:

Scott Jiang

Category:

N/A     Fixed In Release:

2013R1

Found In Release:

2013R1     Status:

Closed

Board:

N/A     Processor:

BF609

Silicon Revision:

    Resolution:

Fixed

Is the bug repeatable?:

N/A     

Summary: spi flash on bf609 ezkit fails to be probed

Details:

 

spi flash on bf609 ezkit fails to be probed now.

 

U-Boot 2013.01 (ADI-2013R1-pre)-00326-gd0a4c06-dirty (Mar 05 2013 - 15:09:09), Build: jenkins-label=UBOOT_BF609-EZKIT-270

 

CPU:   ADSP bf609-0.0 (Detected Rev: 0.0) (parallel flash boot)

Board: ADI BF609 EZ-Kit board

       Support: http://blackfin.uclinux.org/

Clock: VCO: 500 MHz, Core: 500 MHz, System0: 83.333 MHz, System1: 83.333 MHz, Dclk: 250 MHz

RAM:   128 MiB

Flash: 16 MiB

MMC:   Blackfin SDH: 0

In:    serial

Out:   serial

Err:   serial

other init

Net:   mii0

Hit any key to stop autoboot:  0

bfin> sf probe 1

SF: Failed to set up slave

Failed to initialize SPI flash at 0:1

bfin>

 

 

Follow-ups

 

--- Scott Jiang                                              2013-04-01 03:25:35

fixed.

 

--- Mingquan Pan                                             2013-04-10 23:39:39

Yes,close.

 

 

 

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

 

File Name     File Type     File Size     Posted By

No Files Were Found

Attachments

    Outcomes