[#7627] Build failed in Jenkins: gnu_bf_release_conf ? MacBookPro #229

Document created by Aaronwu Employee on Sep 26, 2013
Version 1Show Document
  • View in full screen mode

[#7627] Build failed in Jenkins: gnu_bf_release_conf ? MacBookPro #229

Submitted By: Sonic Zhang

Open Date

2013-02-18 20:54:40     Close Date

2013-03-27 03:41:12

Priority:

Medium     Assignee:

Sonic Zhang

Category:

N/A     Fixed In Release:

N/A

Found In Release:

2013R1     Status:

Closed

Board:

N/A     Processor:

BF609

Silicon Revision:

    Resolution:

Out of Date

Is the bug repeatable?:

N/A     

Summary: Build failed in Jenkins: gnu_bf_release_conf ? MacBookPro #229

Details:

 

.  Failure happens during u-boot build:

 

cc -Wall -Wstrict-prototypes -O2 -fomit-frame-pointer -idirafter /Volumes/GNU-Work/jenkins/workspace/gnu_bf_release_conf/gnu_bf_release/MacBookPro/u-boot/include -idirafter /Volumes/GNU-Work/jenkins/workspace/gnu_bf_release_conf/gnu_bf_release/MacBookPro/u-boot_build/include2 -idirafter /Volumes/GNU-Work/jenkins/workspace/gnu_bf_release_conf/gnu_bf_release/MacBookPro/u-boot_build/include -I /Volumes/GNU-Work/jenkins/workspace/gnu_bf_release_conf/gnu_bf_release/MacBookPro/u-boot/lib/libfdt -I /Volumes/GNU-Work/jenkins/workspace/gnu_bf_release_conf/gnu_bf_release/MacBookPro/u-boot/tools -DCONFIG_SYS_TEXT_BASE= -DUSE_HOSTCC -D__KERNEL_STRICT_NAMES   -o /Volumes/GNU-Work/jenkins/workspace/gnu_bf_release_conf/gnu_bf_release/MacBookPro/u-boot_build/tools/aisimage.o aisimage.c -c

In file included from aisimage.c:29:

/Volumes/GNU-Work/jenkins/workspace/gnu_bf_release_conf/gnu_bf_release/MacBookPro/u-boot/include/image.h:37:27: error: asm/byteorder.h: No such file or directory

 

Follow-ups

 

--- Sonic Zhang                                              2013-02-20 05:36:43

Enable MMC only when MMC_SPI is defined.

Plesae disable MMC_SPI when testing NAND driver.

 

--- Sonic Zhang                                              2013-02-20 05:37:49

Ignore last comments.

 

--- Sonic Zhang                                              2013-02-20 06:21:55

Fixed.

File "include/image.h" should not includes asm headers when built by

HOST_CC.

 

--- Sonic Zhang                                              2013-02-20 06:37:53

Ignore last comments.

 

--- Sonic Zhang                                              2013-02-20 22:40:33

Can replicated on u-boot trunk

 

--- Mingquan Pan                                             2013-03-27 04:48:12

uboot can build for bf609-ezkit. Close.

 

 

 

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

 

File Name     File Type     File Size     Posted By

No Files Were Found

Attachments

    Outcomes