[#7486] mmc test always fails in regression test

Document created by Aaronwu Employee on Sep 26, 2013
Version 1Show Document
  • View in full screen mode

[#7486] mmc test always fails in regression test

Submitted By: Mingquan Pan

Open Date

2012-11-02 01:03:25     Close Date

2013-05-16 02:54:26

Priority:

Medium     Assignee:

Sonic Zhang

Category:

N/A     Fixed In Release:

2012R2-RC3

Found In Release:

2012R2-RC3     Status:

Closed

Board:

N/A     Processor:

BF609

Silicon Revision:

    Resolution:

Duplicated

Is the bug repeatable?:

N/A     

Summary: mmc test always fails in regression test

Details:

 

mmc test always fails in regression test.

 

bfin> mmc rescan 0

sending CMD2 failed

bfin> mmcinfo

sending CMD2 failed

Device: Blackfin SDH

Manufacturer ID: 0

OEM: 0

Name: Tran Speed: 0

Rd Block Len: 0

SD version 2.0

High Capacity: No

Capacity: 0 Bytes

Bus Width: 1-bit

bfin> fatls mmc 0

sending CMD2 failed

MMC: block number 0x1 exceeds max(0x0)

 

** Unable to use mmc 0:1 for fatls **

bfin> reset�

 

U-Boot 2012.07-rc2 (ADI-2012R1-pre)-00269-g983a603-dirty (Oct 31 2012 - 14:34:34), Build: jenkins-label=UBOOT_BF609-EZKIT-231

 

CPU:   ADSP bf609-0.0 (Detected Rev: 0.0) (parallel flash boot)

Board: ADI BF609 EZ-Kit board

       Support: http://blackfin.uclinux.org/

Clock: VCO: 500 MHz, Core: 500 MHz, System0: 83.333 MHz, System1: 83.333 MHz, Dclk: 250 MHz

RAM:   128 MiB

Flash: 16 MiB

MMC:   Blackfin SDH: 0

In:    serial

Out:   serial

Err:   serial

other init

Net:   mii0

Hit any key to stop autoboot:  0

bfin>

 

 

 

Follow-ups

 

--- Sonic Zhang                                              2012-11-26 21:39:21

This error is reported when the sd card is not formated.

Not a bug.

 

--- Mingquan Pan                                             2013-05-16 04:01:43

Duplicated with 6851. Close.

 

 

 

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

 

File Name     File Type     File Size     Posted By

No Files Were Found

Attachments

    Outcomes