[#7280] autoboot countdown test fail now on trunk head

Document created by Aaronwu Employee on Sep 26, 2013
Version 1Show Document
  • View in full screen mode

[#7280] autoboot countdown test fail now on trunk head

Submitted By: Mingquan Pan

Open Date

2012-08-23 01:35:48     Close Date

2012-09-06 01:40:28

Priority:

Medium     Assignee:

steven miao

Category:

N/A     Fixed In Release:

2012R2-RC3

Found In Release:

2012R2-RC3     Status:

Closed

Board:

N/A     Processor:

BF609

Silicon Revision:

    Resolution:

Fixed

Is the bug repeatable?:

N/A     

Summary: autoboot countdown test fail now on trunk head

Details:

 

autoboot countdown test fail now on trunk head.

 

U-Boot 2012.07-rc2 (ADI-2012R1-pre)-00259-gef5d0ff-dirty (Aug 22 2012 - 18:52:05), Build: jenkins-label=UBOOT_BF609-EZKIT-215^M

^M

CPU:   ADSP bf609-0.0 (Detected Rev: 0.0) (parallel flash boot)^M

Board: ADI BF609 EZ-Kit board^M

       Support: http://blackfin.uclinux.org/^M

Clock: VCO: 500 MHz, Core: 500 MHz, System0: 100 MHz, System1: 100 MHz, Dclk: 250 MHz^M

RAM:   128 MiB^M

Flash: 16 MiB^M

MMC:   Blackfin SDH: 0^M

In:    serial^M

Out:   serial^M

Err:   serial^M

other init^M

Net:   mii0^M

Hit any key to stop autoboot:  9 ^H^H^H 8 ^H^H^H 7 ^H^H^H 6

*****************************

STEP 3: Test countdown time period

 

^H^H^H 5 ^H^H^H 4 ^H^H^H 3 ^H^H^H 2 ===== Recording measurement: one boot countdown second is .723971

autoboot second timing is 0.27602899999999997 seconds off

 

===== Recording result: autoboot countdown seconds is fail

 

 

Follow-ups

 

--- steven miao                                              2012-08-31 06:51:54

drop pre-defined clock macros

 

--- Mingquan Pan                                             2012-09-06 02:40:43

Yes. passed. Close.

 

 

 

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

 

File Name     File Type     File Size     Posted By

No Files Were Found

Attachments

    Outcomes