[#7236] bdinfo show wrong braud rate

Document created by Aaronwu Employee on Sep 26, 2013
Version 1Show Document
  • View in full screen mode

[#7236] bdinfo show wrong braud rate

Submitted By: Mingquan Pan

Open Date

2012-08-10 01:05:13     Close Date

2012-08-23 01:29:29

Priority:

Medium     Assignee:

Bob Liu

Category:

N/A     Fixed In Release:

2012R1

Found In Release:

2012R1     Status:

Closed

Board:

N/A     Processor:

BF609

Silicon Revision:

    Resolution:

Fixed

Is the bug repeatable?:

N/A     

Summary: bdinfo show wrong braud rate

Details:

 

bdinfo show wrong braud rate on trunk head.

 

expecting memstart of   0x00000000

expecting memsize of    128*1024*1024

expecting flashstart of 0xb0000000

expecting flashsize of  0x01000000

expecting baudrate of   57600

 

bdinfo^M

U-Boot      = U-Boot 2012.07-rc2 (ADI-2012R1-pre)-00251-gf66e648-dirty (Aug 10 2012 - 11:20:28)^M

CPU         = bf609-0.0^M

Board       = bf609-ezkit^M

VCO         =     25 MHz^M

CCLK        =    500 MHz^M

SCLK        =    100 MHz^M

boot_params = 0x00000000^M

memstart    = 0x00000000^M

memsize     = 0x08000000^M

flashstart  = 0xB0000000^M

flashsize   = 0x01000000^M

flashoffset = 0x00000000^M

ethaddr     = 00:E0:22:FE:87:7E^M

ip_addr     = 10.100.4.50^M

baudrate    = 0 bps^M

bfin> bdinfo memstart result: pass

bdinfo memsize result: pass

bdinfo flashstart result: pass

bdinfo flashsize result: pass

bdinfo ethaddr result: pass

bdinfo ip_addr result: pass

bdinfo baudrate result: fail

 

Follow-ups

 

--- Bob Liu                                                  2012-08-13 02:57:16

fixed, add back baudrate to bdinfo.

 

--- Mingquan Pan                                             2012-08-23 02:27:55

Yes. Close.

 

 

 

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

 

File Name     File Type     File Size     Posted By

No Files Were Found

Attachments

    Outcomes