[#7200] update to2012R1-RC1-BF60x uboot , kernel fails to run ptp case

Document created by Aaronwu Employee on Sep 26, 2013
Version 1Show Document
  • View in full screen mode

[#7200] update to2012R1-RC1-BF60x uboot , kernel fails to run ptp case

Submitted By: Mingquan Pan

Open Date

2012-07-12 03:01:47     Close Date

2012-07-12 21:59:10

Priority:

Medium     Assignee:

Bob Liu

Category:

N/A     Fixed In Release:

N/A

Found In Release:

N/A     Status:

Closed

Board:

N/A     Processor:

BF609

Silicon Revision:

    Resolution:

Fixed

Is the bug repeatable?:

N/A     

Summary: update to2012R1-RC1-BF60x uboot , kernel fails to run ptp case

Details:

 

update to2012R1-RC1-BF60x uboot , kernel fails to run ptp case on 10.99.29.102.

It looks the current ptp kernel booted up have ping problem with the updated uboot, while the default-configured kernel or the previous uboot have no this issue. (Hardware ethernet connection here is good)

 

The worked uboot:

 

U-Boot 2011.09-00203-gd254f76-dirty (ADI-2012R1-pre) (Mar 02 2012 - 17:07:26)^M

^M

CPU:   ADSP bf609-0.0 (Detected Rev: 0.0) (spi flash boot)^M

Board: ADI BF609 EZ-Kit board^M

       Support: http://blackfin.uclinux.org/^M

Clock: VCO: 25 MHz, Core: 500 MHz, System0: 100 MHz, System1: 100 MHz, Dclk: 250 MHz^M

RAM:   128 MiB^M

 

RAM size is 128 MB

Flash: ## Unknown flash on Bank 1 - Size = 0x00000000 = 0 MB^M

0 Bytes^M

MMC:   Blackfin SDH: 0^M

SF: Detected W25Q32 with page size 4 KiB, total 4 MiB^M

In:    serial^M

Out:   serial^M

Err:   serial^M

KGDB:  [on serial] ready^M

Net:   mii0^M

Hit any key to stop autoboot:  5 ^H^H^H 0 ^M

bfin> set console ttyBF0,57600^M

bfin> set bootargs root=/dev/mtdblock0 rw ip=10.100.4.50 earlyprintk=serial,uart0,57600 console=${console}^M

bfin> set serverip 10.100.4.174^M

 

 

 

Follow-ups

 

--- Bob Liu                                                  2012-07-12 05:55:23

fixed,use different MAC address

 

--- Mingquan Pan                                             2012-07-12 22:58:55

Yes, it works now. Close.

 

 

 

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

 

File Name     File Type     File Size     Posted By

No Files Were Found

Attachments

    Outcomes