[#7188] uboot takes serveral miniutes to reset now

Document created by Aaronwu Employee on Sep 26, 2013
Version 1Show Document
  • View in full screen mode

[#7188] uboot takes serveral miniutes to reset now

Submitted By: Mingquan Pan

Open Date

2012-07-06 04:58:48     Close Date

2012-07-09 04:21:46

Priority:

Medium     Assignee:

Nobody

Category:

N/A     Fixed In Release:

N/A

Found In Release:

N/A     Status:

Closed

Board:

N/A     Processor:

BF609

Silicon Revision:

    Resolution:

N/A

Is the bug repeatable?:

N/A     

Summary: uboot takes serveral miniutes to reset now

Details:

 

uboot takes serveral miniutes to reset now.

 

reset   - Perform RESET of the CPU^M

run     - run commands in an environment variable^M

saveenv - save environment variables to persistent storage^M

setenv  - set environment variables^M

sf      - SPI flash sub-system^M

sleep   - delay execution for some time^M

source  - run script from memory^M

strings - display strings^M

tftpboot- boot image via network using TFTP protocol^M

usb     - USB sub-system^M

usbboot - boot from USB device^M

version - print monitor, compiler and linker version^M

bfin> reset^M

failed reset attempt

Attempting to recover to u-boot prompt

^M

^M

U-Boot 2011.09-dirty (ADI-2012R1) (Jul 02 2012 - 20:18:53), Build: jenkins-label=UBOOT_BF609-EZKIT-171^M

^M

CPU:   ADSP bf609-0.0 (Detected Rev: 0.0) (parallel flash boot)^M

Board: ADI BF609 EZ-Kit board^M

       Support: http://blackfin.uclinux.org/^M

Clock: VCO: 25 MHz, Core: 500 MHz, System0: 100 MHz, System1: 100 MHz, Dclk: 250 MHz^M

RAM:   128 MiB^M

Flash: 16 MiB^M

MMC:   Blackfin SDH: 0^M

In:    serial^M

Out:   serial^M

Err:   serial^M

other init^M

Net:   mii0^M

Hit any key to stop autobogot autoboot prompt

ot:  5 ^H^H^H 0 ^M

 

Follow-ups

 

--- Sonic Zhang                                              2012-07-06 06:40:47

fixed

 

--- Mingquan Pan                                             2012-07-09 05:21:43

Yes, close.

 

 

 

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

 

File Name     File Type     File Size     Posted By

No Files Were Found

Attachments

    Outcomes