[#6867] flash post test fails on bf537

Document created by Aaronwu Employee on Sep 26, 2013
Version 1Show Document
  • View in full screen mode

[#6867] flash post test fails on bf537

Submitted By: Mingquan Pan

Open Date

2011-11-04 00:27:38     Close Date

2013-05-16 01:34:45

Priority:

Medium     Assignee:

Nobody

Category:

N/A     Fixed In Release:

2011R1

Found In Release:

2011R1     Status:

Closed

Board:

N/A     Processor:

BF537

Silicon Revision:

    Resolution:

N/A

Is the bug repeatable?:

N/A     

Summary: flash post test fails on bf537

Details:

 

flash post test fails on bf537.

 

I have tried on two bf537 boards both with sw6 all on., but with different fails.

 

bfin> diag run flash

POST flash

        sector 11: 0x20080000 +0x10000

.. done

9....8....7....6....5....4....3....2....1....   sector 12: 0x20090000 +0x10000

.. done

9....8....7....6....5....4....3....2....1....   sector 13: 0x200a0000 +0x10000

.. done

9....8....7....6....5....4....3....2....1....   sector 14: 0x200b0000 +0x10000

.. done

9....8....7....6....5....4....3....2....1....   sector 15: 0x200c0000 +0x10000

.. done

9....8....7....6....5....4....3....2....1....   sector 16: 0x200d0000 +0x10000

.. done

9....8....7....6....5....4....3....2....1....   sector 17: 0x200e0000 +0x10000...

 

..

9....8....7....6....5....4....3....2....1....   sector 63: 0x203c0000 +0x10000

.. done

9....8....7....6....5....4....3....2....1....   sector 64: 0x203d0000 +0x10000

.. done

9....8....7....6....5....4....3....2....1....   sector 65: 0x203e0000 +0x10000- Warning: 1 protected sectors will not be erased!

. done

9....8....7....6....5....4....3....2....1....   sector 66: 0x203f0000 +0x10000- Warning: 1 protected sectors will not be erased!

. done

9....8....7....6....5....4....3....2....1....   sector 67: 0x0 +0x0

.. done

        sector 68: 0x0 +0x0

.. done

        sector 69: 0x0 +0x0

.. done

malloc(0x1010101) failed

...

 

 

U-Boot 2011.09-00094-g90f84a3-dirty (ADI-2011R1) (Nov 04 2011 - 10:35:10)

 

CPU:   ADSP bf537-0.2 (Detected Rev: 0.2) (bypass boot)

Board: ADI BF537 stamp board

       Support: http://blackfin.uclinux.org/

Clock: VCO: 500 MHz, Core: 500 MHz, System: 125 MHz

RAM:   64 MiB

post/post.c: post_time_ms seems not to be implemented

Flash: 4 MiB

MMC:  

In:    serial

Out:   serial

Err:   serial

KGDB:  [on serial] ready

Net:   bfin_mac

Hit any key to stop autoboot:  0

bfin> diag run flash

POST flash

        sector 11: 0x20040000 +0x10000- Warning: 2 protected sectors will not be erased!

done

9Flash not Erased

FAILED

bfin> diag run flash

POST flash

        sector 11: 0x20040000 +0x10000- Warning: 2 protected sectors will not be erased!

done

Flash not Erased

FAILED

bfin> reset�

 

FAILED

bfin>

..

 

Follow-ups

 

--- Mingquan Pan                                             2013-05-16 02:42:02

It can pass in the 2012R2 release. close.

 

 

 

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

 

File Name     File Type     File Size     Posted By

No Files Were Found

Attachments

    Outcomes