[#6425] Can't load image in SPI MMC for latest u-boot

Document created by Aaronwu Employee on Sep 26, 2013
Version 1Show Document
  • View in full screen mode

[#6425] Can't load image in SPI MMC for latest u-boot

Submitted By: Vivi Li

Open Date

2010-12-27 03:54:20    

Priority:

Medium     Assignee:

Sonic Zhang

Category:

N/A     Fixed In Release:

N/A

Found In Release:

2011R1     Status:

Open

Board:

N/A     Processor:

BF537

Silicon Revision:

    Resolution:

Not reproducible

Is the bug repeatable?:

N/A     

Summary: Can't load image in SPI MMC for latest u-boot

Details:

 

Can't load image in SPI MMC for latest u-boot.

 

Last passed version is 2010.12-svn2559 first failed version is 2010.12-svn2567.

 

On bf537-stamp:

--

U-Boot 2010.12-svn2572 (ADI-2011R1-pre) (Dec 27 2010 - 14:58:09)

 

CPU:   ADSP bf537-0.2 (Detected Rev: 0.2) (bypass boot)

Board: ADI BF537 stamp board

       Support: http://blackfin.uclinux.org/

Clock: VCO: 400 MHz, Core: 100 MHz, System: 50 MHz

RAM:   64 MiB

Flash: 4 MiB

MMC:

In:    serial

Out:   serial

Err:   serial

KGDB:  [on serial] ready

Net:   bfin_mac

Hit any key to stop autoboot:  0

bfin> mmc_spi 4

MMC_SPI: 0 at 0:4 hz 25000000 mode 0

bfin> mmcinfo

Device: MMC_SPI

Manufacturer ID: 3

OEM: 5344

Name: SD256

Tran Speed: 25000000

Rd Block Len: 512

SD version 2.0

High Capacity: No

Capacity: 252968960

Bus Width: 1-bit

bfin> fatls mmc 0:1

  4863066   uimage

 

1 file(s), 0 dir(s)

 

bfin> fatload mmc 0 0x1000000 uimage

** Can't read from device 0 **

 

** Unable to use mmc 0:1 for fatload **

bfin>

--

 

Follow-ups

 

--- Sonic Zhang                                              2010-12-30 05:06:59

Can't replicate on svn 2567 and head.

 

 

 

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

 

File Name     File Type     File Size     Posted By

No Files Were Found

Attachments

    Outcomes