[#6069] Unable to use mmc for fatls on bf518f-ezbrd

Document created by Aaronwu Employee on Sep 25, 2013
Version 1Show Document
  • View in full screen mode

[#6069] Unable to use mmc for fatls on bf518f-ezbrd

Submitted By: Vivi Li

Open Date

2010-06-17 02:38:03     Close Date

2010-06-21 22:49:34

Priority:

Medium     Assignee:

Mike Frysinger

Category:

N/A     Fixed In Release:

N/A

Found In Release:

N/A     Status:

Closed

Board:

Ezbrd     Processor:

BF518

Silicon Revision:

    Resolution:

Fixed

Is the bug repeatable?:

N/A     

Summary: Unable to use mmc for fatls on bf518f-ezbrd

Details:

 

MMC can not work on bf518f-ezbrd.

 

Last passed version is 2010.03-svn2283.

First failed version is 2010.03-svn2310.

 

--

U-Boot 2010.03-svn2330 (ADI-2010R1-pre) (Jun 17 2010 - 07:12:21)

 

CPU:   ADSP bf518-0.0 (Detected Rev: 0.0) (parallel flash boot)

Board: ADI BF518F EZ-Board board

       Support: http://blackfin.uclinux.org/

Clock: VCO: 400 MHz, Core: 400 MHz, System: 80 MHz

RAM:   64 MB

Flash:  4 MB

MMC:  Blackfin SDH: 0

In:    serial

Out:   serial

Err:   serial

KGDB:  [on serial] ready

Net:   bfin_mac

Hit any key to stop autoboot:  0

bfin>

bfin> mmc rescan 0

bfin> fatls mmc 0

 

** Unable to use mmc 0:1 for fatls **

bfin>

--

 

Follow-ups

 

--- Mike Frysinger                                           2010-06-21 16:53:20

blah, the portmux pin defines didnt work the way i thought for bf51x.  should be

fixed in trunk now.

 

--- Vivi Li                                                  2010-06-21 22:46:50

OK now.

Close it.

 

 

 

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

 

File Name     File Type     File Size     Posted By

No Files Were Found

Attachments

    Outcomes