[#6067] u-boot parallel image for bf526-ezbrd can not boot in trunk now

Document created by Aaronwu Employee on Sep 25, 2013
Version 1Show Document
  • View in full screen mode

[#6067] u-boot parallel image for bf526-ezbrd can not boot in trunk now

Submitted By: Vivi Li

Open Date

2010-06-12 05:50:11     Close Date

2010-06-21 18:46:22

Priority:

Medium     Assignee:

Mike Frysinger

Category:

N/A     Fixed In Release:

N/A

Found In Release:

N/A     Status:

Closed

Board:

N/A     Processor:

BF527

Silicon Revision:

    Resolution:

Duplicated

Is the bug repeatable?:

N/A     

Summary: u-boot parallel image for bf526-ezbrd can not boot in trunk now

Details:

 

Update u-boot parallel image for bf526-ezbrd, it fails to boot up.

The last passed version is U-Boot 2010.03-svn2281.

 

--

U-Boot 2008.10-svn2133 (ADI-2009R1.1-rc1) (Dec  4 2009 - 14:22:14)

 

CPU:   ADSP bf526-0.0 (Detected Rev: 0.0) (spi flash boot)

Board: ADI BF526 EZ-Board board

       Support: http://blackfin.uclinux.org/

Clock: VCO: 400 MHz, Core: 400 MHz, System: 80 MHz

RAM:   64 MB

Flash:  4 MB

SF: Got idcode bf 25 04

In:    serial

Out:   serial

Err:   serial

Net:   Blackfin EMAC

MAC:   00:E0:22:FE:0F:1B

Hit any key to stop autoboot:  0

bfin>

bfin> tftp 0x1000000 u-boot.bin

Using Blackfin EMAC device

TFTP from server 10.100.4.174; our IP address is 10.100.4.50

Filename 'u-boot.bin'.

Load address: 0x1000000

Loading: ##############

done

Bytes transferred = 201208 (311f8 hex)

bfin> go 0x1000000

## Starting application at 0x01000000 ...

 

 

U-Boot 2010.03-svn2323 (ADI-2010R1-pre) (Jun 12 2010 - 17:06:28)

 

CPU:   ADSP bf526-0.0 (Detected Rev: 0.0) (parallel flash boot)

Board: ADI BF526 EZ-Board board

       Support: http://blackfin.uclinux.org/

Clock: VCO: 400 MHz, Core: 400 MHz, System: 80 MHz

RAM:   64 MB

Flash:  4 MB

In:    serial

Out:   serial

Err:   serial

KGDB:  [on serial] ready

Warning: Generating 'random' MAC address

Net:   bfin_mac

Hit any key to stop autoboot:  0

bfin> printenv

bootargs=root=/dev/mtdblock0 rw clkin_hz=25000000 earlyprintk=serial,uart1,57600 console=ttyBF1,57600

bootcmd=run ramboot

bootdelay=5

baudrate=57600

loads_echo=1

ipaddr=192.168.0.15

serverip=192.168.0.2

autoload=no

rootpath=/romfs

gatewayip=192.168.0.1

netmask=255.255.255.0

hostname=bf526-ezbrd

loadaddr=0x1000000

nc=set ncip ${serverip};set stdin nc;set stdout nc

ubootfile=u-boot.ldr

update=tftp $(loadaddr) $(ubootfile);protect off 0x20000000 +$(filesize);erase 0x20000000 +$(filesize);cp.b $(loadaddr) 0x200000)

addip=set bootargs $(bootargs) ip=$(ipaddr):$(serverip):$(gatewayip):$(netmask):$(hostname):eth0:off

ramfile=uImage

ramargs=set bootargs root=/dev/mtdblock0 rw clkin_hz=25000000 earlyprintk=serial,uart1,57600 console=ttyBF1,57600

ramboot=tftp $(loadaddr) $(ramfile);run ramargs;run addip;bootm

nfsfile=vmImage

nfsargs=set bootargs root=/dev/nfs rw nfsroot=$(serverip):$(rootpath),tcp,nfsvers=3

nfsboot=tftp $(loadaddr) $(nfsfile);run nfsargs;run addip;bootm

flashboot=bootm 0x20100000

stdin=serial

stdout=serial

stderr=serial

ethaddr=fa:c4:df:91:80:83

ethact=bfin_mac

 

Environment size: 1098/8188 bytes

bfin> set ipaddr 10.100.4.50

bfin> set serverip 10.100.4.174

bfin> set gatewayip 10.100.4.174

bfin> run update

Using bfin_mac device

TFTP from server 10.100.4.174; our IP address is 10.100.4.50

Filename 'u-boot.ldr'.

Load address: 0x1000000

Loading: ###############

done

Bytes transferred = 209916 (333fc hex)

........... done

Un-Protected 11 sectors

 

........... done

Erased 11 sectors

Copy to Flash... done

bfin> reset

(change to parallel boot mode and reset, fail to boot)

--

 

Follow-ups

 

--- Mike Frysinger                                           2010-06-21 18:42:15

dupe of [#6068]

 

 

 

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

 

File Name     File Type     File Size     Posted By

No Files Were Found

Attachments

    Outcomes