Seeing Amplifier Resistor Sizing Tradeoffs with Signal Chain Designer

When designing an amplifier, setting the gain is often the first thing engineers focus on. The math is straightforward: pick a feedback resistor ratio and you’re done.  However in practice, the actual resistor values you choose can quietly make or break the design.

The Challenge: Same Gain, Different Performance

For a non‑inverting amplifier, the closed‑loop gain is defined by a simple relationship:


Non-Inverting Amplifier Gain Formula

Many resistor pairs result in the same gain. However, absolute resistor values introduce real‑world tradeoffs. Noise, input offset, bandwidth, and output loading can all shift in subtle ways that aren’t obvious from hand calculations alone.

This is where the Signal Chain Designer (SCD)  tool can help, by making these performance tradeoffs visible early in the design process.

Visualizing Resistor Size Effects with Signal Chain Designer

Signal Chain Designer allows you to explore how resistor sizing affects both an individual amplifier stage and the full signal chain by interactively adjusting the feedback resistor values. Here's a sneak peek at the parameters you can configure in the amplifier block.

Configuring Amplifier Stage in Signal Chain Designer

As resistor values change, you can immediately see the impact on:

  • Noise performance - Larger resistors increase thermal noise, which can dominate in low‑noise signal chains.
  • Input bias current effects - High‑value resistors magnify offset errors caused by input bias currents.
  • Bandwidth and frequency response - Parasitic capacitances interact with resistor values, affecting stability and usable bandwidth.
  • Output loading and drive stress - Very small resistor values increase output current demand and power dissipation.

These effects are real, but they’re easy to overlook when the focus is only on achieving the correct gain. Relying on equations alone makes it easy to push resistor values too far in either direction ( "Too Large" or "Too Small") without fully realizing the impact. With the tool, it is much easier to understand why extreme resistor choices are risky and where performance starts to degrade for a given op amp.

Here are several scenarios  how Signal Chain Designer shows the effects of amplifier resistor sizing on key design performance parameters.

Visualizing Resistor Size Effect in Gain with Signal Chain Designer

Visualizing Resistor Size Effect in Noise with Signal Chain Designer

Visualizing Resistor Size Effect in Power with Signal Chain Designer


Evaluating feedback resistor sizing is especially valuable when designing low‑noise or high‑precision signal chains, interfacing with high‑impedance sensors, operating near bandwidth or stability limits, or troubleshooting unexpected noise, offset, or performance loss despite correct gain calculations.

In these cases, resistor sizing is a critical design choice, not something to leave to trial and error. Signal Chain Designer enables designers to vary amplifier feedback resistor values and immediately observe the system‑level impact. This visibility helps identify a practical operating range for a given op amp and application.

To learn more about how Signal Chain Designer evaluates amplifier resistor sizing, check out this intuitive walkthrough video: Signal Chain Designer: Amplifier Resistor Sizing.