Post Go back to editing

DC current in capacitor with srcsteps=0

Category: Software
Software Version: 26.0.2

Good day,

I hit a minor problem when using .option srcsteps=0, that is, choosing to disable the DC convergence method that steps the independent sources.

With srcsteps=0, when the feedback capacitor is below about 1uF, there is no current flowing in resistors R1 and R4 after the DC operating point is found, no problem.

For higher values of capacitor, a wild current is following in these resistors, while the capacitor current marker remains as zero and the node voltages are bad.

This behaviour does not occur when the opamps are not present, that is, with passive components only.

So there is some extreme non-linear connection between opamps and capacitors.

On one hand, the .option srcsteps=0 is scarcely needed.

On the other hand, I have been forced to use this option with similar opamp circuits with high loop gain and with some opamps, such as the AD8065, which tend to latch up when reduced source voltage is permitted.

Could the good folk at ADI confirm this behaviour ?  Please advise if I am doing something wrong.

Best regards. 

Capacitor DC current with srcsteps=0.asc

LTspice 26.0.2 for Windows
Circuit: E:\LTSpice\BProbe\Capacitor DC current with srcsteps=0.net
Start Time: Wed Nov  4 18:36:50 2026
Options:srcsteps=0 gfarad=0
solver = Alternate
Maximum thread count: 8
tnom = 27
temp = 27
method = trap
Compress1stOrder = true
Compress2ndOrder = true
Direct Newton iteration failed to find operating point.
Starting Gmin stepping
Gmin stepping failed to find operating point. Use".option gminsteps=0" to skip all Gmin stepping.
Source stepping method for .op point skipped.
Starting Gmin stepping level 2
Gmin stepping level 2 failed to find operating point. Use".option gminsteps=0" to skip all Gmin stepping.
Source stepping method for .op point skipped.
Pseudo transient terminated at 100.654 s, solution accepted ready or not!
Total elapsed time: 0.795 seconds.

Files loaded:
E:\LTSpice\BProbe\Capacitor DC current with srcsteps=0.net
C:\Users\Chris\AppData\Local\LTspice\lib\sub\AD8065.sub
C:\Users\Chris\AppData\Local\LTspice\lib\sub\ADA4523-1.sub
LTspice 26.0.2 for Windows
Circuit: E:\LTSpice\BProbe\Capacitor DC current with srcsteps=0.net
Start Time: Wed Nov  4 18:39:49 2026
Options:srcsteps=2 gfarad=0
solver = Alternate
Maximum thread count: 8
tnom = 27
temp = 27
method = trap
Compress1stOrder = true
Compress2ndOrder = true
Direct Newton iteration failed to find operating point.
Starting Gmin stepping
Gmin stepping failed to find operating point. Use".option gminsteps=0" to skip all Gmin stepping.
Starting source stepping with srcstepmethod=0
Source stepping succeeded in finding the operating point.

Total elapsed time: 0.275 seconds.

Files loaded:
E:\LTSpice\BProbe\Capacitor DC current with srcsteps=0.net
C:\Users\Chris\AppData\Local\LTspice\lib\sub\AD8065.sub
C:\Users\Chris\AppData\Local\LTspice\lib\sub\ADA4523-1.sub

Parents Reply Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.