Post Go back to editing

Simulation Issues with T-Type Three-Level Inverters Using IGBTs

Category: Software
Product Number: LTspice
Software Version: 26.0.2

Hello,

Recently i enocuntered a problem with Simulation Issues with T-Type Three-Level Inverters Using IGBTs.

This is the topology diagram of a T-type three-level converter.

I‘m analyzing the power decoupling circuit of a T-type three-level inverter and I have observed voltage spikes during the turn-off of the vertical-leg switch(Taking QT1 as an example); however, the experimental results do not align with the LTSpice simulations.

Waveform at the moment of vertical pipe shut-off

This is the oscilloscope waveform captured at the moment the vertical-leg switch turns off. Channel 1 shows Vge of the vertical-leg switch(QT1), Channel 2 shows Vce of the vertical-leg switch(QT1),Channel 3 displays the current flowing through its collector (C) pin(QT1), and Channel 4 shows Vce of the horizontal-leg switch(QT3), which operates complementarily to the vertical-leg switch.

In this experimental waveform, the turn-off voltage of the IGBT does not exhibit the high-frequency oscillations typically seen with MOSFETs.

To predict the voltage spike that occurs when the vertical-leg switch turns off, I set up a simulation of a T-type three-level inverter in LTspice.

Single_Phase_Loop_Test_Different_Gate_Driver_Resistance.asc

However, in the simulation I set up, high-frequency oscillations appear in the turn-off voltage of the vertical pipe (U1). I have determined that these oscillations are caused by the interaction between the parasitic inductance I introduced and the output capacitance Coes of the switching device.

This is the LTspice model download link I downloaded from the Infineon official website.

https://www.infineon.cn/document-promo/infineon-spice-l1-igbt-1200v-trenchstop-igbt7-s7-simulationmodels-en_0938b21b-d878-4672-a088-dd85af861b08

https://www.infineon.cn/document-promo/infineon-spice-l1-igbt-650v-trenchstop5-s5-simulationmodels-en_3ac7fa12-cdaf-403e-9ced-33b2e062eab0

The first question is: why does this high-frequency oscillation not appear in the IGBT experiment, whereas it does appear in the MOSFET experiment?

The second question is: what are the remaining flaws in my simulation model, and how can I achieve better agreement with the experimental results?

Thanks a lot!

Looking forward to your reply.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.