I am running a simulation envolving an NMOS LEVEL3 model from cmosedu.com (for teaching purposes).
KCC's Quizzes AQQ305 about a mutual exponentiation equation
1. Quote of the month: "A train station is where a train stops. A bus station is where a bus stops. I have a work station on my desk, so..." - unknown
2. Quiz AQQ305 about finding a mutual exponential equation
Good luck, and try to be among the
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
LTspice
Production
LTspice® is a powerful, fast, and free SPICE simulator software, schematic capture and waveform viewer with enhancements and models for improving the simulation...
LTspice on Analog.com
Dear pifouille ,
Thank you for bringing this to our attention. The root cause of the discrepancy you observed is a bug in the MOS3 model code which LTspice inherited from spice3. It'll be fixed in the next release.
I haven't checked myself, but it would appear that ngspice (also based on spice3) had this already corrected.
Meanwhile, you can work around it by setting VMAX=0 in the .model card, if this is acceptable to you.
Best Regards,
Mathias
Hi mborn, and thank you for your reply.
Thanks for the tip too. With VMAX=0, I do get the same value in both analyses.
It's off by about 30% though (10uS instead of 7.5u).
Anyway, that's fine for me.
Thanks again.
Pif.
PS: In my initial post, I meant that I got gds in ngspice by printing @M1[gds] and not @M1[gm], obviously