Post Go back to editing

BV input sources

Category: Software
Product Number: LTSP
Software Version: 26.1.1

I have made a symbol type X´that is a transistor with 3 pins called u1

When I try to use BV with Ix(u1:2) it is not possible can not find instance.

The trace window show alternatives Ix(u1:2) but i can not use it in the schematics

It is not a big issue for me but I tell it

Parents
  • Hi  ,

    Pin currents cannot be called on by behavioral sources. B sources, in simulation, have access to time-stepped node voltages and (two-pin) device currents. A pin is neither a node, nor a device. There is a trick, though: add a 0V voltage source at the pin as a current probe and reference its current I(V1) in your B source. You can rotate the polarity of the 0V source to produce the signed current as desired.

    mike

Reply
  • Hi  ,

    Pin currents cannot be called on by behavioral sources. B sources, in simulation, have access to time-stepped node voltages and (two-pin) device currents. A pin is neither a node, nor a device. There is a trick, though: add a 0V voltage source at the pin as a current probe and reference its current I(V1) in your B source. You can rotate the polarity of the 0V source to produce the signed current as desired.

    mike

Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.