First of all, thank you for the release of V26.1.1 and for the continued improvements to LTspice.
I noticed some behavior in V26.1.1 regarding the interpretation of `FROM` / `TO` in the `.meas` command that appears to be different from previous versions.
The attached sample circuit is a very simple test case.
A transient analysis is run for 50 ms, with data saved starting from 20 ms.
Therefore, the waveform viewer displays a time range of 0 to 30 ms.
I then use `.meas` commands to calculate the AC RMS value.
In previous versions, my understanding has been that the times specified by `FROM` / `TO` correspond to the time axis displayed in the waveform viewer.
With that interpretation, I would expect the following results from these three measurements:
Measurement "out1_mean" FAIL'ed
Measurement "out1_acrms" FAIL'ed
out2_mean: AVG(v(out))=2.57779e-006 FROM 0.02 TO 0.03
out2_acrms: RMS(v(out) - out2_mean)=0.703621 FROM 0.02 TO 0.03
out3_mean: AVG(v(out))=0 FROM 0.01 TO 0.02
out3_acrms: RMS(v(out) - out3_mean)=0 FROM 0.01 TO 0.02
However, in V26.1.1, I actually get the following results:
out1_mean: AVG(V(out))=4.32692331062e-06 FROM 0 TO 0.05
out1_acrms: RMS(V(out) - out1_mean)=0.405740403021 FROM 0 TO 0.05
out2_mean: AVG(V(out))=0 FROM 0.02 TO 0.03
out2_acrms: RMS(V(out) - out2_mean)=0 FROM 0.02 TO 0.03
Measurement "out3_mean" FAIL'ed
Measurement "out3_acrms" FAIL'ed
From these results, it appears that `FROM` / `TO` in V26.1.1 are being interpreted using a different time reference from previous versions. However, I am unable to understand exactly which time interval is being measured.
Is this an intentional change in V26.1.1, or could this be an issue?
Best regards,
Denspa
Edit Notes
Translated Title to English. Removed contains AI generated content flag. Added keywords.[edited by: MStokowski at 5:50 PM (GMT -4) on 20 Oct 2026]