Post Go back to editing

LTspice 26.0.2 for MacOs uses too much memory

Category: Software
Product Number: LTspice
Software Version: 26.0.2

With the update from LTspice 17 to 26 on macOS, LTspice now includes many features from the Windows release. However, memory usage has increased significantly. A simple CMOS inverter using the sky130A PDK (translated from ngspice to ltspice): RAM usage has increased from 100MB to 1GB! As circuit complexity increases, RAM usage increases hugely, up to 5Gb for only 5 inverters!

I imagine that, to update LTspice to the same Windows version, designers may have needed to use Rosetta 2, but I would like to ask whether this huge memory increase is expected behavior. With these memory requirements, I may no longer be able to use LTspice on macOS.

I am simulating the CMOS_Inverter circuit in the sky130A folder from my repository
https://github.com/Torr250/Analog-ICDesign-OpenTools/tree/main/LTspice/sky130A 

Parents
  • LTspice uses more RAM as I open schematics; even after I close a schematic, RAM usage stays high. As I open a new schematic, RAM keeps increasing. It seems LTspice never releases RAM.

    Starting LTspice at idle consumes around 270MB of RAM; as I open and close example schematics, the RAM usage keeps increasing:

    Idle: 273MB

    Schematic 1: 315MB

    Schematic 2: 431MB

    Schematic 3: 556MB

    Schematic 4: 660MB

    Schematic 5: 790MB

    Schematic 6: 911MB

    Schematic 7: 1,016MB

    Blank Schematic: 1.1GB

    These are only opening and closing schematics, not even simulating them.

     

     

     

     

     

     

     

Reply
  • LTspice uses more RAM as I open schematics; even after I close a schematic, RAM usage stays high. As I open a new schematic, RAM keeps increasing. It seems LTspice never releases RAM.

    Starting LTspice at idle consumes around 270MB of RAM; as I open and close example schematics, the RAM usage keeps increasing:

    Idle: 273MB

    Schematic 1: 315MB

    Schematic 2: 431MB

    Schematic 3: 556MB

    Schematic 4: 660MB

    Schematic 5: 790MB

    Schematic 6: 911MB

    Schematic 7: 1,016MB

    Blank Schematic: 1.1GB

    These are only opening and closing schematics, not even simulating them.

     

     

     

     

     

     

     

Children

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.