Post Go back to editing

I have various computers, Windows 11 ( working using 26.1) and also Windows 10 Pro, 26.1 will not load... My actual request is to know when LTSPICE will be released for Mac OS 27...? A lot to ask, but Mac's are my daily machines, running latest O

Thread Summary

The user inquires about the availability of LTSpice for Mac OS 27. The final answer confirms that LTSpice will run as before, but Rosetta is no longer installed automatically. Users can manually install Rosetta to run Intel-based apps, and Analog Devices is working on an Apple Silicon version due to the planned end-of-life for Rosetta in OS 28.
AI Generated Content
Category: Software
Product Number: LTSPICE
Software Version: LTSpice latest release for Mac will not run on MAcOS 27.xxx

Hoping for a timely release of LTSpice for Mac OS 27... running the same GUI is a huge benefit... but alas not yet on MacOS 27. 

Thanks! 

Parents
  • Hi  ,

    It will run, and is supported as before, but it appears Rosetta is no longer installed automatically with MacOS 27. You can still follow Apple's instructions to install Rosetta:

    support.apple.com/.../102527

    We are working on an Apple Silicon version, as we are well aware of the imminent end-of-life for Intel-based apps support via Rosetta. Apple claims this will happen OS 28. Clearly, Apple is trying to preempt the user experience by throwing circus hoops in front of users who simply need Rosetta.

    In sum, the support is no different than it was for OS 26.x, just Apple made it harder.

    mike

  • Mike:  Thanks for the prompt responss, just FYI, I have a Macbook M2MAX, so not Intel, thus Rosetta does not help. 

    I'll just wait for the OS27 version...   Windows 11 runs fine... Windows 10 Pro.. just wont open, despite trying the various suggested reloads and configs... 

    Thanks,   Steve

  • Hi  ,

    Mike:  Thanks for the prompt responss, just FYI, I have a Macbook M2MAX, so not Intel, thus Rosetta does not help. 

    Actually, Rosetta does just the opposite of what you infer: it enables Intel binaries (software), such as LTspice64 Windows, to run on Apple Silicon, i.e., M-series Macs, ostensibly allowing older Mac x86 software to run on ARM64 macs. This was to ease the transition of Mac i9 users such as myself to use the intel-based software I already had on my M3 while devs worked to catch up. Rosetta has the beneficial side effect of allowing ported Windows x86 apps to run on an M-based mac via crossover or other means.

    So, install Rosetta, and you should be able to use LTspice 26.0. You will probably get a dire warning message that you can do so, but also call the developer and scold them; the latter bit you have done. :-)

    Right now, we are in a world where LTspice supports both x86 Windows machines and ARM64 Windows machines. LTspice x86 or x86_64 was very portable between Windows and Mac, since these OSs used the same underlying chip architecture. Now, we have returned (back to 2006) to a world where underlying architectures are very different: Windows ARM to Mac ARM is not really a thing. The ARM goals are different between the two worlds. Windows ARM machines are typically cheaper and battery-efficient laptops, sold as lower performance machines, whereas your M2MAX is a performance beast, and designed to be so. 

    Mike

Reply
  • Hi  ,

    Mike:  Thanks for the prompt responss, just FYI, I have a Macbook M2MAX, so not Intel, thus Rosetta does not help. 

    Actually, Rosetta does just the opposite of what you infer: it enables Intel binaries (software), such as LTspice64 Windows, to run on Apple Silicon, i.e., M-series Macs, ostensibly allowing older Mac x86 software to run on ARM64 macs. This was to ease the transition of Mac i9 users such as myself to use the intel-based software I already had on my M3 while devs worked to catch up. Rosetta has the beneficial side effect of allowing ported Windows x86 apps to run on an M-based mac via crossover or other means.

    So, install Rosetta, and you should be able to use LTspice 26.0. You will probably get a dire warning message that you can do so, but also call the developer and scold them; the latter bit you have done. :-)

    Right now, we are in a world where LTspice supports both x86 Windows machines and ARM64 Windows machines. LTspice x86 or x86_64 was very portable between Windows and Mac, since these OSs used the same underlying chip architecture. Now, we have returned (back to 2006) to a world where underlying architectures are very different: Windows ARM to Mac ARM is not really a thing. The ARM goals are different between the two worlds. Windows ARM machines are typically cheaper and battery-efficient laptops, sold as lower performance machines, whereas your M2MAX is a performance beast, and designed to be so. 

    Mike

Children

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.