Hi,
I would like to plot the input capacitance (and the input resistance) of a jfet source follower circuit in the function of frequency . The input impedance is complex of course in the frequency range involved between 1 MHz and 10 MHz but I need help in doing this.
I used the 2N4416 jfet model and its input capacitance is known from data sheet (which is about 3-4 pF) but I wish to see it plotted on the vertical axis while the horizontal axis shows the frequency range.
Here is the schematic I use for simulation, together with the small signal AC simulation plot on the voltage output and I attached the asc circuit file too

JFET source follower tests 1.asc
Thanks for any help in advance.
Gyula