Post Go back to editing

Plotting JFET source follower input capacitance in the function of frequency

Thread Summary

The user seeks to plot the input capacitance and resistance of a JFET source follower circuit (2N4416) over a frequency range of 1 MHz to 10 MHz. The final answer provides a method to calculate the input capacitance using the formula Ig(J1)/(V(ugs)*2*3.1454*frequency), resulting in 16.2 pF at 1 MHz. However, the user notes that this value seems high compared to the datasheet, which specifies Cgs as 2.41 pF and Cgd as 1.6 pF.
AI Generated Content
Category: Software
Software Version: LTspice (x64): 26.0.2

Hi,

I would like to plot the input capacitance (and the input resistance) of a jfet source follower circuit in the function of frequency .   The input impedance is complex of course in the frequency range involved between 1 MHz and 10 MHz but I need help in doing this. 

I used the 2N4416 jfet model and its input capacitance is known from data sheet (which is about 3-4 pF) but I wish to see it plotted on the vertical axis while the horizontal axis shows the frequency range. 

Here is the schematic I use for simulation, together with the small signal AC simulation plot on the voltage output and I attached the asc circuit file too

JFET source follower tests 1.asc

Thanks for any help in advance. 

Gyula

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.