Post Go back to editing

Errors importing OPA814 SUBCKT model from Texas Instruments.

Thread Summary

The user encountered errors when trying to simulate the OPA814 opamp from Texas Instruments in LTSpice due to unsupported syntax in the .lib file. The final answer suggests replacing the lines with .ends directives that include pin names (e.g., .ends OPA814 IN+ IN- OUT V+ V-) with a simple .ends. The OPA814 model and LTSpice configuration were discussed.
AI Generated Content
Category: Software
Product Number: LTSpice
Software Version: 26.0.2

I have put together an amplifier circuit that uses the AD811 that simulates properly.

I would like to try using the Texas Instruments opamp OPA814 instead.

I downloaded the official model from the TI website:

https://www.ti.com/product/OPA814#tech-docs

Link to file, I renamed to .lib for consistency with some other custom parts (they work fine).

https://www.ti.com/lit/zip/SBOMCE1

When I look at this file in a text editor, it looks pretty good. Not encrypted, looks like a standard SUBCKT to me, with the only exception being that the pin order is

.subckt OPA814 IN+ IN- OUT V+ V-

instead of the LTSpice opamp model that has IN+ IN- V+ V- OUT.

I put this file into my working folder and imported it with spice directive

.LIB OPA814_Model_V1p1.lib

to match the filename in the working folder.

I placed a opamp2 symbol, made the value OPA814 to match the name in the .subsck definition in the library file, and ctl-clicked the part to check the prefix is X and the Value is OPA814. 

When I then try to simulate it, I get errors like the following:

C:\Dropbox\Spice Files\High Voltage Amplifier\OPA814_Model_V1p1.lib(222): Expected device instantiation or directive here.
.ends OPA814 IN+ IN- OUT V+ V-
^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^
C:\Dropbox\Spice Files\High Voltage Amplifier\OPA814_Model_V1p1.lib(255): Expected device instantiation or directive here.
.ends FEMT_0 1 2

To me this says that the .lib file is being read, but it is upset about the lines starting with .ends. In the library file these lines are unremarkable to me and I am not sure how to correct the error, however the mentioned line numbers are the lines that have those directives.

I know that I will have to figure out how to also correct the pin ordering, but for now it seems like a library parsing issue. Could you please help me to fix the library parsing to avoid this error?

OPA814_Model_V1p1.libexample.asc

Parents Reply Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.