Post Go back to editing

Spice Model doesn't work, is there a fix?

Category: Hardware
Product Number: LT3081

The LT3081 model doesn't seem to work when configured for higher input voltages. The DEMO is fine at 5V, but when using 10-25V the output stays at 5.8V or so independent of the programing resistor. Making simple changes to the DEMO circuit shows this behavior. I see that this is true on several other forums, so is there a fix for this? If not, would you send me sample parts to hardware test? 

Thanks,

Rob Verity

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.