Hi all,
I am trying to install LTspice in my new work laptop with the following specifcations -
- Processor Intel(R) Core(TM) Ultra 5 125H (3.60 GHz)
- Installed RAM 24.0 GB (23.5 GB usable)
- Graphics card Intel(R) Graphics (128 MB)
- System type 64-bit operating system, x64-based processor
- Edition Windows 11 Home Single Language
- Version 25H2
- OS build 26200.9168
The installation completes without any error shown on the screen but the software does not launch. I have tried several LTspice versions starting from 24.1 and the issue is the same. I tried installing the software using all the 3 options - 'For user', 'For all' and 'Server. Based on some old answers describing a similar issue I have generated and attached the installation log file for your reference when installing version 26.0.2 for user installation. Please let me know how i can fix the same.