Post Go back to editing

Discrepancy between LTspice conducted EMI simulation and LTpowerCAD/Reference EMI profiles for LT8610

Category: Hardware
Product Number: LTspice

Hi everyone,

I am currently developing an LT8610-based buck converter and using LTspice for pre-compliance conducted EMI simulation. I am employing a symmetrical LISN setup and have integrated parasitic models (ESR/ESL) for the input capacitors (CinB, CinC) along with common-mode coupling paths (C_stray) to simulate the noise environment.

Current Methodology:

  • Simulation: Transient analysis with a Hanning-windowed FFT.

  • Analysis: I am using standard LISN matrix decomposition to isolate noise modes: $V_{DM} = V_1 - V_2$ and $V_{CM} = V_1 + V_2$.

Observation:

While my simulation successfully captures the fundamental switching harmonics, my total conducted emissions peak at approximately 45 dBµV. This is significantly lower than the 80–90 dBµV peaks typically seen in reference EMI profiles or LTpowerCAD predictions for similar topologies.

Questions:

  1. Measurement Point: Is this amplitude discrepancy primarily due to the fact that I am measuring at the filter output (attenuated), whereas reference charts often display source noise (unattenuated)?

  2. Parasitic Modeling: What is the industry-standard approach in LTspice to accurately model PCB trace inductance and loop area to align simulated "source" noise levels with reference design data?

  3. Switching Dynamics: Are there specific non-ideal switching models or parameters for the LT8610 internal MOSFETs that I should be incorporating to more accurately represent high-frequency common-mode energy contributions?

I would appreciate any guidance on how to bridge this delta between my simulated filter output and theoretical reference EMI profiles.

Best regards,

Varad

Parents
  • Hi  ,

    I am currently developing an LT8610-based buck converter and using LTspice for pre-compliance conducted EMI simulation.

    That is a big lift for LTspice. This is not its strong suit. LTpowerCAD is far better at this job, as the templates/calculations have been tested and verified against real world EMI results.LTpowerCAD has this advantage over LTspice, where the inner workings of the device are mapped as behavioral results as opposed to time step simulated.

    • Measurement Point: Is this amplitude discrepancy primarily due to the fact that I am measuring at the filter output (attenuated), whereas reference charts often display source noise (unattenuated)?

    • Parasitic Modeling: What is the industry-standard approach in LTspice to accurately model PCB trace inductance and loop area to align simulated "source" noise levels with reference design data?

    • Switching Dynamics: Are there specific non-ideal switching models or parameters for the LT8610 internal MOSFETs that I should be incorporating to more accurately represent high-frequency common-mode energy contributions?

    Probably yes to all? And more, likely. Again, this is a steep hill to climb. 

    Note: You have three (somehow, moderated) postings of this thread. I will delete the others.

    mike

  • 1

    hey Mike, 

    thank you for Response. 

    varad

Reply Children
No Data