LTspice
Production
LTspice® is a powerful, fast, and free SPICE simulator software, schematic capture and waveform viewer with enhancements and models for improving the simulation...
LTspice on Analog.com
Hello,
I observed some strange behavior in the .meas Statement Editor. The menu appears when right-clicking on a .meas statement.Eg :

I want to measure the power (U × I) when voltage V1 falls to 2.5 V for the first time.
The measurement seems to work correctly when I click ‘Test’, and the LTspice log file is generated properly

.meas function again, I lose the previous .meas Statement Editor window, and the configuration is different. .meas statement seems to not be interpreted.
Is it a bug?
I also notice sometime after running the simulation when I clic on "test" button in the .meas Statement Editor "error" but in reality function works fine in log file. I have to log this kind of behaviour.
Emilien
Hi esabard38V2 ,
I checked this out. It seems to replace the When with At. Bug has been around forever...
mike
Hi esabard38V2 ,
I checked this out. It seems to replace the When with At. Bug has been around forever...
mike