Post Go back to editing

LTSpice 26 minor bug when .NOISE points to wrong current source

Thread Summary

The user encountered an LTSpice crash when using the .NOISE command incorrectly on a short-circuited current source. The support engineer confirmed the issue and will report it. For voltage sources with series resistors, the .NOISE command does not crash and correctly outputs zero noise.
AI Generated Content
Category: Software
Product Number: LTSpice 26
Software Version: LTSpice 26

This is a highly unlikely simulation situation, and hardly needs fixing.

I swapped between two current sources, using a short circuit across the current source that was momentarily not wanted.  Then when the .NOISE command was used, but incorrectly pointing to the short circuited current source, LTSpice crashed.  If the same thing is done with voltage sources + series resistors, the .NOISE output doesn't crash and gives zero noise, which is the expected result.

 Debug I.asc

Parents Reply Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.