Post Go back to editing

LTspice S-parameters extraction with dependant sources.

Category: Software
Software Version: 24.0.12

Hi! 

I have a huge model in a library that I created for a customer. The model is based on voltage dependent voltage sources to emulate Laplace Transforms. I did a simplification of the problem in the picture below because the problem is the same at the entire model scale. Why can't I do an S-parameter extraction in the circuit 2 if both circuits are practically the same? Am I missing something in the model of E1? Or is it just a LTspice limitation? Arr the input ports from E1 considered as a n open circuit and that's why S11 = 0dB? Thanks in advance!

Forum_question.zip

Edit Notes

Nothing special
[edited by: alanum21 at 8:57 PM (GMT -4) on 1 Jun 2026]