LTspice
Production
LTspice® is a powerful, fast, and free SPICE simulator software, schematic capture and waveform viewer with enhancements and models for improving the simulation...
LTspice on Analog.com
Hello to the community.
Please comment on the following use case. I have a design to simulate. And this design has a BAS70 diode in it. The standard library doesn't have it, so I decided to import a SPICE model found on the Net. It is not a problem. All I have to do is to put it in the "standard.dio" usually found in the "C:\Users\$USER_NAME$\Local\LTspice\lib\cmp" directory" (Windows 10).
The problem is I plan to share this design with other members of the team. So asking them to update their libraries is not that convenient. Instead I decided to put all the design-specific models in the same directory the schematic resides, like this:
After that, it is enough to specify these "sym" and "sub" directories in the "Search Paths" tab of the settings, like presented in the figure below. Quite convenient. Per my taste, of course.

==========
This works fine for the relatively complex components, like "subcircuits": there is a "component.asy" in the "sym" directory and its model "component.sub" in the "sub". Connection is established using the "ModelFile" attribute.

==========
But here is a quirk. A diode is a pretty simple device, covered by a single .model SPICE directive. There is no need to create a subcircuit for it. So I decided to stick to the following approach:
It seemed to me the best and most straightforward approach: a self-contained symbol with no external dependencies.

==========
Unfortunately, it didn't work. Attempt to simulate a very basic schematic yields the following error:

Check on the netlist gives the following:
* \PowerOld\root.asc
* Generated by LTspice 26.0.2 for Windows.
V1 N001 0 SINE(0 12 50)
R1 N002 0 10K
D1 N001 N002 .model BAS70 D(IS=99.5p RS=0.600 BV=70.0 IBV=10.0u CJO=2.00p M=0.333 N=1.70 TT=7.20n) BAS70
.model D D
.lib C:\Users\ \AppData\Local\LTspice\lib\cmp\standard.dio
.tran 0.2
.backanno
.end
==========
One may see that the value of the attribute "SpiceMode" is attached immediately after the list of the nodes of the "D1" component. It is illegal for SPICE. The ".model" must be found somewhere in the code on a distinct line. I tried different combinations of the symbol's attributes, but neither gave an expected result.
It is possible, though, to overcome this limitation by placing the SPICE directive directly on the schematic, like this:

This way the netlist is correct and the simulation concludes.
* \PowerOld\root.asc
* Generated by LTspice 26.0.2 for Windows.
V1 N001 0 SINE(0 12 50)
R1 N002 0 10K
D1 N001 N002 BAS70
.model D D
.lib C:\Users\\AppData\Local\LTspice\lib\cmp\standard.dio
.tran 0.2
.model BAS70 D(IS=99.5p RS=0.600 BV=70.0 IBV=10.0u CJO=2.00p M=0.333 N=1.70 TT=7.20n)
.backanno
.end
==========
So is this behavior expected? Or is it a bug? Or maybe I misunderstood the purpose of the "SpiceModel" field? Yes, it is possible to workaround this problem either by creating a subcircuit or placing the .model directly on the schematic. But both are less convenient than what I was expecting.
Thanks for your attention.
Cool, that works! Thanks for the advice.
Putting the ".model" directives might be the "most portable" option for sure. But it messes up the schematic itself. There is a plain netlist for this type of information. So the solution you proposed suits me better.
=====
And I have to say that this topic is poorly covered in the existing help/documentation. In particular, as you have already noticed, the "SpiceModel" and "ModelFile" attributes are not distinct enough, if you ask me. You said, that :
>> "spicemodel" is looking for a .subckt, not a .model.
But the "ModelFile" actually does the same.
As an example. If I want to import the LM2903 comparator, I do the following:

Some clarification or a few real-world examples would be welcomed to clear outline how to use the "SpiceModel" and "ModelFile" attributes correctly. And of course, the reference to the "Symbol and Library Search Paths" chapter so a newcomer would be able to quickly untangle this knot.
=====
Consider this message as more of feedback but complain. :-)
Hi ElShang ,
Some clarification or a few real-world examples would be welcomed to clear outline how to use the "SpiceModel" and "ModelFile" attributes correctly. And of course, the reference to the "Symbol and Library Search Paths" chapter so a newcomer would be able to quickly untangle this knot.
No argument there. It could use some work. Check out the Help > FAQs > Third Party Models.
But the "ModelFile" actually does the same.
Well, yes, and no. ModelFile is specifically for a .sub or .lib file name. This attribute produces a .lib statement in the netlist. This is editable in the symbol, but not on a schematic. Some libraries containing a number of subcircuits, the actual subckt line is called by SpiceModel or Value. Either works, but not both. A symbol's attributes (other than prefix, description, and ModelFile) are simply used to build the spiceline for the component. Not too fancy.
As an example. If I want to import the LM2903 comparator, I do the following:
- create the "$SOME_PATH/sym/LM2903.asy" symbol;
- create the "$SOME_PATH/sub/LM2903.sub", which contains the implementation of the LM2903 in the form of the ".subckt";
- update the "Symbol Search Paths" and "Simulation Library Search Paths" so they point to the "$SOME_PATH/sym/" and "$SOME_PATH/sub/" respectively;
Yes, that is one way. Note that for symbols, you simply need to define $SOME_PATH/ in Search Paths, as search is recursive (when you open a schematic or click Refresh in the Place Component dialog). In contrast, subcircuits do require the full path, as you state.
If your intent is portability, I might suggest a slightly different path, using new features of 26.0.2. Below would be the complete method of creating the symbol for an LM2903.


That's it. :-)
Now, for portability, always send the symbol and library along with the schematic in the same directory.
That said, you could set up your local libraries as you wish, but remember to package up any files you would need. You can quickly check what symbols and libraries are used by simply Choosing View > Update and View SPICE Netlist.

mike
No argument there. It could use some work. Check out the Help > FAQs > Third Party Models.
Yep, I've got it. Thanks for the clue. The concept of "user.*" libraries for the basic components is indeed mentioned there. Hope that someone will find this thread and stick to this approach.
This attribute produces a .lib statement in the netlist.

If your intent is portability, I might suggest a slightly different path, using new features of 26.0.2.

Hi ElShang ,
And that's a better explanation. I eventually dove into the "raw" SPICE syntax, so it is nice to know which LTspice's primitive/text fields correspond to which SPICE's directive. By the way, original SPICE3 3f3 documentation does not mention the ".lib" directive, only ".include". And LTspice's help index for some reasons doesn't list it as well, though it is described in the "LTspice Simulator/Dot Commands" chapter.
I believe LTspice has had the library directive for quite some time. .lib and .include are functionally equivalent, except for the section feature (below).
And LTspice's help index for some reasons doesn't list it as well
I should fix the index…
I eventually dove into the "raw" SPICE syntax, so it is nice to know which LTspice's primitive/text fields correspond to which SPICE's directive.
Yes, once you understand that the attributes are just building out a spiceline, it makes much more sense.
ModelFile becomes .lib "Filename"
Description is not used
All other attributes are simply placed in line on the spice netlist
Prefix§Instance [Nodes…] SpiceModel Value Spiceline1…
Typically, the actual model is put in the Value field, since that usually defaults to visible.
Agreed the attribute names are non-ideal.
By the way, in regard to the ".lib" directive. Could you, probably, explain what does "section" syntax means?The path to the library is obvious. But what is the "entryname". The name of the component? Like "Take this only this component out of the library and put it into the netlist"? But what for?
You can have a library (section) within the library and only load that section. So, for instance, in the file called MyLibrary.lib you might have:
****** Sections in MyLibrary.lib *****
**** section_1 ****
.lib section_1
subckt foo 1 2 3
....netlist
ends
subckt bar 1 2 3
....netlist
ends
.endl
**** section_2 ****
.lib section_2
subckt foo 1 2 3
....other netlist
ends
subckt bar 1 2 3
....other netlist
ends
.endl
In your schematic you would have:
.lib "MyLibrary.lib" section_2
This would only load the second library.
Note that you can also use this syntax in a symbol's ModelFile attribute. Be sure to use quotes for the filename.
mike
Hi ElShang ,
And that's a better explanation. I eventually dove into the "raw" SPICE syntax, so it is nice to know which LTspice's primitive/text fields correspond to which SPICE's directive. By the way, original SPICE3 3f3 documentation does not mention the ".lib" directive, only ".include". And LTspice's help index for some reasons doesn't list it as well, though it is described in the "LTspice Simulator/Dot Commands" chapter.
I believe LTspice has had the library directive for quite some time. .lib and .include are functionally equivalent, except for the section feature (below).
And LTspice's help index for some reasons doesn't list it as well
I should fix the index…
I eventually dove into the "raw" SPICE syntax, so it is nice to know which LTspice's primitive/text fields correspond to which SPICE's directive.
Yes, once you understand that the attributes are just building out a spiceline, it makes much more sense.
ModelFile becomes .lib "Filename"
Description is not used
All other attributes are simply placed in line on the spice netlist
Prefix§Instance [Nodes…] SpiceModel Value Spiceline1…
Typically, the actual model is put in the Value field, since that usually defaults to visible.
Agreed the attribute names are non-ideal.
By the way, in regard to the ".lib" directive. Could you, probably, explain what does "section" syntax means?The path to the library is obvious. But what is the "entryname". The name of the component? Like "Take this only this component out of the library and put it into the netlist"? But what for?
You can have a library (section) within the library and only load that section. So, for instance, in the file called MyLibrary.lib you might have:
****** Sections in MyLibrary.lib *****
**** section_1 ****
.lib section_1
subckt foo 1 2 3
....netlist
ends
subckt bar 1 2 3
....netlist
ends
.endl
**** section_2 ****
.lib section_2
subckt foo 1 2 3
....other netlist
ends
subckt bar 1 2 3
....other netlist
ends
.endl
In your schematic you would have:
.lib "MyLibrary.lib" section_2
This would only load the second library.
Note that you can also use this syntax in a symbol's ModelFile attribute. Be sure to use quotes for the filename.
mike
You can have a library (section) within the library and only load that section. So, for instance, in the file called MyLibrary.lib you might have:
Good, I've got it.
Probably this is a feature to reduce a netlist size? It would be nice to have this mentioned in the help. I mean a few words about the "section" syntax.
In fact LtSpice's help is already quite good, don't get me wrong. I've got attached to the SPICE syntax exactly using it, though I never became a "true" hardware designer. :-) It just feels a little neglected and outdated. Somewhere there are the screenshots mentioning the LTspice XIV, or something like that.