Post Go back to editing

s-parameter using LTspice

Thread Summary

The user is trying to generate S-parameters (.s2p file) for the LTC6419 using LTspice, specifically for differential output. The final answer suggests using the V(ref) option in the .NET command, such as '.net V(out[,ref]) ...', to correctly simulate the differential output and obtain accurate S11, S12, S21, and S22 data.
AI Generated Content
Category: Software
Product Number: LTC6419
Software Version: LTspice ver 24.1.8


Hello

My customer want to get S-parameter (.s2p) for LTC6419, but there are no S-parameter.

So, I will try to have s2p file from LTspice simulation using .NET command.

However, I don't know the syntax in case of differential output, not single end output.


syntax ( singel end output)  syntax ;

.NET V(out) VIN Rin=50 Rout=50

When I use E1 component in order to change differential to single end, simulation result of S12 is -210dB.( please refer tp attached)


Would you please let me know the way to have simulation using .NET command in case differential output?

I want to have correct S11/S12/S21/S22 data in order to have s2p file.

Best Regards

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.