Post Go back to editing

NE555 model RST not working

Category: Software
Product Number: LTspice
Software Version: 26.0.1

I'm using the NE555 model in a mono-stable configuration.  The datasheet for the NE555 suggests that placing a LOW level on the RST pin will immediately reset the output to LOW and (discharge the RC network).  However, when I place a LOW on the model's RST pin, it does nothing.  Am I misunderstanding this functionality or is this model missing this Fast_Attack_Adj_Delay_v2.op.raw

LTspice 26.0.1 for Windows
Circuit: C:\Users\Instrument\Documents\LTspice\Fast_Attack_Adj_Delay_v2.net
Start Time: Wed May  6 05:39:52 2026
solver = Normal
Maximum thread count: 8
tnom = 27
temp = 27
method = trap
Direct Newton iteration failed to find operating point.
Starting Gmin stepping
Gmin stepping succeeded in finding the operating point.

Total elapsed time: 0.096 seconds.

Files loaded:
C:\Users\Instrument\Documents\LTspice\Fast_Attack_Adj_Delay_v2.net
C:\Users\Instrument\AppData\Local\LTspice\lib\cmp\standard.dio
C:\Users\Instrument\AppData\Local\LTspice\lib\sub\NE555.sub

Fast_Attack_Adj_Delay_v2.ascFast_Attack_Adj_Delay_v2.rawfunctionality?  Do you have a suggestion for a LTSpice component model that includes this functionality? 

Parents Reply Children
No Data