I'm using the NE555 model in a mono-stable configuration. The datasheet for the NE555 suggests that placing a LOW level on the RST pin will immediately reset the output to LOW and (discharge the RC network). However, when I place a LOW on the model's RST pin, it does nothing. Am I misunderstanding this functionality or is this model missing this Fast_Attack_Adj_Delay_v2.op.raw
LTspice 26.0.1 for Windows Circuit: C:\Users\Instrument\Documents\LTspice\Fast_Attack_Adj_Delay_v2.net Start Time: Wed May 6 05:39:52 2026 solver = Normal Maximum thread count: 8 tnom = 27 temp = 27 method = trap Direct Newton iteration failed to find operating point. Starting Gmin stepping Gmin stepping succeeded in finding the operating point. Total elapsed time: 0.096 seconds. Files loaded: C:\Users\Instrument\Documents\LTspice\Fast_Attack_Adj_Delay_v2.net C:\Users\Instrument\AppData\Local\LTspice\lib\cmp\standard.dio C:\Users\Instrument\AppData\Local\LTspice\lib\sub\NE555.sub